Do you have some benchmark data of i.MX6DL GPU with OpenCL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Do you have some benchmark data of i.MX6DL GPU with OpenCL?

跳至解决方案
2,060 次查看
satoshishimoda
Senior Contributor I

Hi community,

Do you have some benchmark data of i.MX6DQ GPU when it is used for GPGPU with OpenCL?

Any benchmark soft is ok, but it is better if the data includes the CPU (Cortex-A9 in i.MX6DQ) performance also to compare CPU vs GPU performance.

Best Regards,

Satoshi Shimoda

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
1,226 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am afraid there is no such official data.

In general one can look at next helpful links

EEMBC -- The Embedded Microprocessor Benchmark Consortium

LMbench Benchmarks on i.MX

Benchmarking the GPU bandwidth capability based on OpenCL memory copy operation | allontutorials

The computing power of the Vivante's GC2000 GPU in i.mx6q (more)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,227 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am afraid there is no such official data.

In general one can look at next helpful links

EEMBC -- The Embedded Microprocessor Benchmark Consortium

LMbench Benchmarks on i.MX

Benchmarking the GPU bandwidth capability based on OpenCL memory copy operation | allontutorials

The computing power of the Vivante's GC2000 GPU in i.mx6q (more)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复