iMX28 enable SPI in Linux 3.10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX28 enable SPI in Linux 3.10

跳至解决方案
1,946 次查看
silviagonzalez
Contributor II

Hello

We’re trying to enable the SPI functionality in an iMX287 with kernel 3.10.

We’ve added the highlighted lines to the imx28-mba28.dts file:

apb@80000000 {

                               apbh@80000000 {

                                             

                                               pinctrl@80018000 {

                                               ...           

                                               };

                               };

                               apbx@80040000 {

                                             

                                              ssp2: ssp@80014000 {

                                                               #address-cells = <1>;

                                                               #size-cells = <0>;

                                                               compatible = "fsl,imx28-spi";

                                                               pinctrl-names = "default";

                                                               pinctrl-0 = <&spi2_pins_a>;

                                                               status = "okay";

                                                               flash: m25p80@0 {

                                                                              #address-cells = <1>;

                                                                              #size-cells = <1>;

                                                                              compatible = "m25p80,fsl,imx28-spi";

                                                                              spi-max-frequency = <40000000>;

                                                                              reg = <0>;

                                                               };

                                               };

                               };

                };

But we’ve found that unless we comment the following highlighted lines in the imx28.dtsi file the compilation fails:

apb@80000000 {

                               apbh@80000000 {

                                               compatible = "simple-bus";

                                               #address-cells = <1>;

                                               #size-cells = <1>;

                                               reg = <0x80000000 0x3c900>;

                                               ranges;

                                               /*ssp2: ssp@80014000 {

                                                               #address-cells = <1>;

                                                               #size-cells = <0>;

                                                               reg = <0x80014000 0x2000>;

                                                               interrupts = <98 84>;

                                                               clocks = <&clks 48>;

                                                               dmas = <&dma_apbh 2>;

                                                               dma-names = "rx-tx";

                                                               fsl,ssp-dma-channel = <2>;

                                                               status = "disabled";

                                               };*/

                                               pinctrl@80018000 {

                                                               #address-cells = <1>;

                                                               #size-cells = <0>;

                                                               compatible = "fsl,imx28-pinctrl", "simple-bus";

                                                               reg = <0x80018000 0x2000>;

                                                             

                                                               spi2_pins_a: spi2@0 {

                                                                              reg = <0>;

                                                                              fsl,pinmux-ids = <

                                                                                              0x2100 /* MX28_PAD_SSP2_SCK__SSP2_SCK */

                                                                                              0x2110 /* MX28_PAD_SSP2_MOSI__SSP2_CMD */

                                                                                              0x2120 /* MX28_PAD_SSP2_MISO__SSP2_D0 */

                                                                                              0x2130 /* MX28_PAD_SSP2_SS0__SSP2_D3 */

                                                                              >;

                                                                              fsl,drive-strength = <1>;

                                                                              fsl,voltage = <1>;

                                                                              fsl,pull-up = <1>;

                                                               };

                                               };

                               apbx@80040000 {

                                               compatible = "simple-bus";

                                               #address-cells = <1>;

                                               #size-cells = <1>;

                                               reg = <0x80040000 0x40000>;

                                               ranges;

                               };

                };

};

Once we comment these lines the compilation is successfully completed but when booting the system we get the following error:

mxs-spi: probe of ssp.5 failed with error -22

Are we missing anything? Could you help us, please?

Thanks in advance for your help.

标签 (2)
0 项奖励
回复
1 解答
1,366 次查看
alejandrolozan1
NXP Employee
NXP Employee
0 项奖励
回复
2 回复数
1,367 次查看
alejandrolozan1
NXP Employee
NXP Employee
0 项奖励
回复
1,366 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Silvia,

The compatible string you use is not correct.

Take a look at this dts file that shows the usage of a m25p80 spi flash on mx28:

https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/arch/arm/boot/dts/imx28-m2...