iMX28 I2C slave Rx functionality issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX28 I2C slave Rx functionality issue

2,783 次查看
zeeshanaslam
Contributor I

Hi,

I am having issues in receiving data from Aardvark master with I2C0 configured as slave on iMx28evk.  I go through following configuration sequence:

  1 - Reset APB DMA controller/Reset and initialize I2C controller

  2 - Determine if its master write request from I2C_STAT register on slave_irq interrupt

  3 - Setup DMA descriptor as follows:

       NXTCMDAR =  0x0

       DMACMD  --   cmd = 0x1 (write),  irq = 1, decsema = 1, chain = 0, wait4endcmd = 1, bytes_count = 1, pio_words = 1

       PIOWRD   --   I2C_RUN | I2C_AKCNOWLEDGE | I2C_RETAIN_CLOCK | 1 (xfer_count)

       Other I2C setting:

       CTRL0_MASTER_MODE - 0x0, CTRL1_ACK_MODE = 0x1, Baud_rate = 400KHz, CTRL1_Slave_Address = 0x87, CTRL1_IRQ_EN= 0xFF (all irq enabled)

  4 - Reset the DMA channel # 6 by asserting reset bit 22 and waiting for it to clear in APB_CTRL reg.

  5 - Starting the DMA channel (by writing dma descriptor address to NXTCMDAR register and INCREMENT_SEMA + 1)

  6 - I recieve 0xFF in rx buffer (Whereas my slave address is 0x43 and data starts with 0xAA) and I2C data_completion interrupt and dma_cmd_completion interrupts are generated. Should I receive slave address as a first byte? I am receiving incorrect byte 0xFF?

  7 - After clearing i2c data_cmplt interrupt I check dma_cmd_cmplt irq to setup next dma commad in the same way (steps 3), again reset the dma and then start it as before. But no activity happens on either dma channel or i2c and things remains stalled. I mean successive dma commands must be processed successfully byte after byte but its not the case.  What I2c interrupts I keep enabled?

Kindly help us identify what is wrong/missing in above mentioned receive processing sequence that DMA command is not processed second time I go through the same steps and configuration. (Although sometimes I have observed this issue on first iteration (preparing fr 1st byte receive) as well). Can this problem be caused because of not being able to reset the APB DMA and channels properly?

Thanks & Regards,

Zeeshan Aslam

标签 (1)
0 项奖励
回复
3 回复数

2,398 次查看
PeterChan
NXP Employee
NXP Employee

Hello Zeeshan Aslam,

In step 6, when the incorrect 0xFF is received as the first byte, what is the value in HW_I2C_DATA register?

In step 7, I don't think you need to reset the DMA channel in the middle of the transaction. Just write the DMA descriptor to HW_APBX_CHx_NEXTCMDAR and increase the HW_APBX_CHx_SEMA will do.

0 项奖励
回复

2,398 次查看
imxcommunitysco
Senior Contributor II

Zeeshan Aslam, has Vladan Jovanovic's answer been helpful? If yes, please select either Correct Answer or Helpful Answer.

Thanks,

Yixing

0 项奖励
回复

2,398 次查看
VladanJovanovic
NXP Employee
NXP Employee

You can check OBDS package on i.MX28 pages for low-level init routines for various modules, including I2C. Might help with locating the issue.