iMX28 : EMI pin keeper function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX28 : EMI pin keeper function

ソリューションへジャンプ
1,705件の閲覧回数
koichisakagami
Contributor II

Dear community,

We design the custom board .
We need information about EMI pin behavior.

The EMI pin is  EMI_ODT1, EMI_CE1N.

The register setting is as follows.
  HW_PINCTRL_MUXSELxx = 11 ( function disable )
  PINCTRL Bank 5/6 Pad Keeper Disable Register = 0 ( enable the internal keeper)

Question1.
  Is the internal keeper function enabled ?

Question2.
  If the "PINCTRL Bank 5/6 Pad Keeper Disable Register"  set as "1" ( disable the internal keeper),
  then, Is the pin state high impedance ?


Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,487件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.

The internal keeper function is enabled.  

According to Figure 9-1 (Pad Diagram) of the i.MX28 Reference Manual

the internal keeper can be enabled / disabled separately, without reference
to multiplexing options.

2.
From section 9.1 (Pin Control and GPIO Overview) :
“All EMI pins' internal keepers can be disabled to allow them to change to

a high impedance state […]”.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,488件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.

The internal keeper function is enabled.  

According to Figure 9-1 (Pad Diagram) of the i.MX28 Reference Manual

the internal keeper can be enabled / disabled separately, without reference
to multiplexing options.

2.
From section 9.1 (Pin Control and GPIO Overview) :
“All EMI pins' internal keepers can be disabled to allow them to change to

a high impedance state […]”.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信