iMX25 WinCE 6 source code.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX25 WinCE 6 source code.

1,211 次查看
andrew_questps
Contributor III

Hi all,

I just have a question regarding whether there is updated source code for the iMX25 BSP after the Dec '09 release. I have notice that in the WCE600_11.04.02_ER_SOURCE (dated 02/02/12) there is support for the iMX25 in the source tree but there is no indication that the platform has actually been tested with it. When I browse to the iMX25 tree on the website the only BSP that is listed for the iMX25 is WCE600_09.12.00_SDK.

Has anyone else used the later source and can verify that it functions correctly with the iMX25 PDK??

Cheers,

Andre

标记 (1)
0 项奖励
回复
0 回复数