iMX25 - Serial Download Documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX25 - Serial Download Documentation

Jump to solution
2,753 Views
bfac
NXP Employee
NXP Employee

Hello,

Our customer is having issues finding a NAND flash memory compatible with our iMX25 device, the NFC is not as flexible as newer ones.

He is trying to connect a MT29F16G08ABABAWP, for which he needs to program the memory with 218 spare bytes, what can be done with success using ATK (that reads back successful), but when trying to boot the board, it fails.

We would like to debug the boot process in more details so we would like to have more documentation on the serial download protocol, so we can have better idea of what is happening.

Chapter 7.8 – "Serial Download Protocol" of RM does not give much debug information, do we have more specific documentation?

BR,

Bruno

0 Kudos
Reply
1 Solution
2,315 Views
PeterChan
NXP Employee
NXP Employee

Hello Bruno,

Chapter 7.9 in RM describes the Serial Download Protocol on i.MX25. The link https://community.freescale.com/docs/DOC-1639 has some examples written by python to show how the SDP works.

Please also read the application note AN3985 "Customizing the Freescale® Advanced Toolkit for i.MX Based Platforms" for supporting new NAND flash device in ATK. The document is available at http://www.freescale.com/

Regards,

Peter

View solution in original post

0 Kudos
Reply
3 Replies
2,315 Views
YixingKong
Senior Contributor IV

Bruno

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply
2,316 Views
PeterChan
NXP Employee
NXP Employee

Hello Bruno,

Chapter 7.9 in RM describes the Serial Download Protocol on i.MX25. The link https://community.freescale.com/docs/DOC-1639 has some examples written by python to show how the SDP works.

Please also read the application note AN3985 "Customizing the Freescale® Advanced Toolkit for i.MX Based Platforms" for supporting new NAND flash device in ATK. The document is available at http://www.freescale.com/

Regards,

Peter

0 Kudos
Reply
2,315 Views
YixingKong
Senior Contributor IV

PeterChan, could you see if you can help this one aftr Easter?
Thanks,

Yixing

0 Kudos
Reply