iMX25-SD Card Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX25-SD Card Boot

跳至解决方案
2,246 次查看
arumugamramasam
Contributor II

Hi,

I have a kit of iMX25-PDK with a CPU, personality Board and a Debug board. I have also taken the reference gerber files from Freescale web and produced the 5 more CPU boards of iMX25 - 3 Stack Configuration. I have loaded the Uboot, uImage and Root file system in SD card (4GB) using a linux ubuntu 9.04 machine and placed the card in the personality board. Original CPU is placed over the personality board and after changing the Dip settings for SD Card booting, it is working.

When I change the CPU board alone with my newly produced CPU board, it is not booting. I don't know what are the steps to be followed when I go for a fresh CPU.

I am not able to conclude whether the newly built hardware CPU is working or not.

If I try with ATK Tool for downloading with Flash type set as SD/MMC, it throws an error message as "Connection Error. Please reset the board and make sure the board in bootstrap mode"

Kindly help if anyone implemented the same way we are working.

Thanks,

Arumugam R

标签 (1)
0 项奖励
回复
1 解答
2,055 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Are you using the same DDR? or different DDR?

If different DDR, you may need to modify the bootloader (e.g. u-boot) and the ATK source code for the DDR.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,056 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Are you using the same DDR? or different DDR?

If different DDR, you may need to modify the bootloader (e.g. u-boot) and the ATK source code for the DDR.

0 项奖励
回复