iMX233 USB connection mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX233 USB connection mode

2,139件の閲覧回数
paolomartinetti
Contributor I

Hi everybody.

i have some problem with my device, 233-equipped, when i plug USB cable first on computer and after in device.

The device-plug probably connects D+/ D- pins before power and ground ones.

Could be this wrong? After this 'bad' connection, my device stops working and seems powered off.

Is there any way to avoid this acting on kernel code?

Thanks in advance

0 件の賞賛
返信
3 返答(返信)

2,016件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Paolo

it is not allowed to apply voltages to unpowered processor.

This can not be configured in software.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,016件の閲覧回数
paolomartinetti
Contributor I

My device is powered with a Li-Ion battery. I attach USB connecting data pins before Power and Ground pins.

0 件の賞賛
返信

2,016件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

it does not matter, if processor is not turned on

(unpowered)

Power-up can be started with one of several events:

PSWITCH pin >= minimum MID level PSWITCH for 100 ms

VDD5V power pin > 4.25 V for 100 ms

0 件の賞賛
返信