iMX clock build failed when disable debugfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX clock build failed when disable debugfs

Jump to solution
2,796 Views
xiongweihuang
Contributor III

Hello all

current git source will miss the CONFIG_CLK_DEBUG in arch/arm/plat-mxc/clock.c

Here is the patch file

Please approve

 

Thanks and regards

Original Attachment has been moved to: clock_dbg.patch.zip

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,411 Views
maheshmahadeva1
NXP Employee
NXP Employee

Thanks for the patch. Makes sense, I will push to integrate into the FSL GIT repo.

Best regards,

-Mahesh

View solution in original post

0 Kudos
Reply
3 Replies
2,411 Views
xiongweihuang
Contributor III

I am glad this is useful

0 Kudos
Reply
2,411 Views
maheshmahadeva1
NXP Employee
NXP Employee

Patch is available on Freescale public GIT at the below link:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.0.35_4.0.0

0 Kudos
Reply
2,412 Views
maheshmahadeva1
NXP Employee
NXP Employee

Thanks for the patch. Makes sense, I will push to integrate into the FSL GIT repo.

Best regards,

-Mahesh

0 Kudos
Reply