i tried to perform stress test on LPDDR4 RAM using mscale ddr tool . but i got struck in middle

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i tried to perform stress test on LPDDR4 RAM using mscale ddr tool . but i got struck in middle

938 次查看
srinivas_123
Contributor III

i am using nxp imx8mplus lpddr4 evk.

i am doing stress test on lpddr4 ram using mscale ddr tool

I follow the steps in guide .

step1 :1. Connect the target board to PC host

step 2:. Launch the MSCALE_DDR_Tool.exe in administrator mode

step3:Press Search button in the Debug UART area, then choose the correct UART port
connected to the MX8 Cortex A-Core Debug UART and press Connect button.

step 4:Load DDR initialization script and choose correct downloading options (select the default one present in script folder)

step 5:Press Download button and wait for target board ready 

in this step I am stuck here . please help me out.

calibration button is not enabled to perform calibrations

error.png

 thanks&Regards

srinivas

0 项奖励
回复
3 回复数

916 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Did you put the board on serial download mode?

Best regards.

0 项奖励
回复

899 次查看
srinivas_123
Contributor III

srinivas_123_0-1716516995282.png

 

yes i kept in serial download => 0001 
i don't why this is happening

please help me 

0 项奖励
回复

892 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Please try with the next script <your_installation_path>\script\mx8mp\mx8mp_lpddr4_2gb_2000m_200m_50m_32bit_2cs_v6.ds

JorgeCas_0-1716560291929.png

JorgeCas_1-1716560300390.png

JorgeCas_2-1716560308532.png

Best regards.

0 项奖励
回复