i.mx93. Using parallel camera and display interface in one device simultaneously.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx93. Using parallel camera and display interface in one device simultaneously.

1,796件の閲覧回数
Serg_mx6
Contributor II

Hello, I want to use i.mx93 series processor (MIMX9352CVUXMAA). I want to connect a camera to it via a parallel 8-bit interface and a display via a parallel 24-bit interface. There was a problem that the processor pins used for the display and the camera intersect (example: Pin J21 using for cam_clk and for disp_clk). Whether correctly I understand, what at the same time these two interfaces cannot be used?

Is there some way around this problem?

For example, remap display or camera pins to other pins?

 

 

0 件の賞賛
返信
2 返答(返信)

1,759件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

The IOMUX and Pad Control Registers are able to change function of the pin and re-map them to another. For this particular case, MEDIAMIX_CAM_CLK and MEDIAMIX_DISP_CLK functions are only mapped to J21 pin.

Best regards.

0 件の賞賛
返信

1,539件の閲覧回数
rameshasp
Contributor IV

Can anyone confirm still MIMX9352CVUXMAA is this part number available in NXP, Digikey, Mouser and Arrow?

 

0 件の賞賛
返信