i.mx93. Using parallel camera and display interface in one device simultaneously.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx93. Using parallel camera and display interface in one device simultaneously.

1,776 次查看
Serg_mx6
Contributor II

Hello, I want to use i.mx93 series processor (MIMX9352CVUXMAA). I want to connect a camera to it via a parallel 8-bit interface and a display via a parallel 24-bit interface. There was a problem that the processor pins used for the display and the camera intersect (example: Pin J21 using for cam_clk and for disp_clk). Whether correctly I understand, what at the same time these two interfaces cannot be used?

Is there some way around this problem?

For example, remap display or camera pins to other pins?

 

 

0 项奖励
回复
2 回复数

1,739 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

The IOMUX and Pad Control Registers are able to change function of the pin and re-map them to another. For this particular case, MEDIAMIX_CAM_CLK and MEDIAMIX_DISP_CLK functions are only mapped to J21 pin.

Best regards.

0 项奖励
回复

1,519 次查看
rameshasp
Contributor IV

Can anyone confirm still MIMX9352CVUXMAA is this part number available in NXP, Digikey, Mouser and Arrow?

 

0 项奖励
回复