i.mx93 Fusebox description

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx93 Fusebox description

3,395 Views
im93user
Contributor I
Dear NXP,
 
I have a few issues with the fusebox descriptions across all available documents for imx93
=================
General questions:
=================
 
IMX93RM_rev4:
 
"Fuses can generally only be set from 0 to 1 and the most common failure is a 1 appearing as a 0. The simplest mechanism to verify 
these failures is redundancy. Redundancy is when two bits are OR'd together so that if either is set, then the output value is a 1.
In case of fuses protected by redundancy, only 16 of the 32 bits are available (bits 15:0 are automatically copied to 31:16) and 
checked on read. This allows for multiple programming operations on a word, so bits can be configured at different times."
 
I haven't found a single fuse in the fusemap xls attached to the RM or in the security RM where this redundancy could have been written into
the shadowregisters.
 
Is that redundancy something that is handled by the ELE fwr?
Which fuses are protected by redundancy?
Does every fuse have to be written through the ELE API or are there any other fuses present that can be
accessed (read\write) without it?
 
=======================================
Questions regarding exact fuse settings:
=======================================
 
 
!BootCFG0!
 
SD Speed Selection/ eMMC bus width:
 
If my boot mode fuses is "internal fuses" and bt_fuse_sel is true, my boot mode will be:
USDHC1 8-bit eMMC 5.1
 
What SD Speed section "0b11 - 8 bit ddr (eMMC 4.4)" or "0b01 - 8bit" eMMC Bus width decides then exactly?
 
 
uSDHC IO Voltage Selection / eMMC Speed Selection / eMMC Bus width:
 
Can these actually set separately? Afaik HS400 eMMC requires all of these to be set:
8 bit DDR, 1.8 V I\O , not sure what high speed means but I'm guessing it sets the clock?
 
 
!BootCFG1!
 
uSDHC Power Cycle Interval
uSDHC Power Cycle Delay
Power Cycle Enable
 
Are these attached to the secondary boot offset somehow?
I thought that the only way to set up let's say a fallback bootloader to an eMMC on the uSDHC is to
specify a fixed offset for it, what the power cycling is\can be used for exactly?
 
uSDHC DLL Enable
uSDHC DLL Select
 
Couldn't find much information in eMMC 5.1 reference manuals for this, how does that work exactly?
 
 
WDOG_Enable
WDOG_Timeout_Select
 
Is the WDOG needed if I'm using a fallback bootloader on an eMMC so that during NORMAL boot mode it can iterate
through primary bootloader -> secondary bootloader -> serial fallback?
 
What feeds the WDOG HW during boot?
 
 
!OEM MAC ADDRESS!
 
315 - WORD
32  - num of fusebits
MAC1_ADDR_31_0[31:0]
 
316 - WORD
16 - num of fusebits
MAC1_ADDR_47_32[47:32]
16 - num of fusebits
MAC2_ADDR_15_0[15:0]
 
317 - WORD
32  - num of fusebits
MAC2_ADDR_47_16[47:16]
 
 
According to the i.MX9 fusemap description the OEM MAC addresses shall be stored in a straight-forward manner, 
and the mainlined nvmem linux drivers are swapping the endianness the MAC Addresses like that.
 
However, the security reference manual describes the exact same fuses the following way:
 
39 word 3  MAC1_ADDR_31_0[15:0]
           MAC1_ADDR_31_0[31:16]
39 word 4  MAC1_ADDR_47_32[47:32]
           MAC2_ADDR_47_32[47:32]
39 word 5  MAC2_ADDR_31_0[15:0]
           MAC2_ADDR_31_0[31:16]
   
Which one is the correct description?
 
 
!SRK HASHES!
 
Based on the RMs are my assumptions correct regarding NXP and OEM SRK hashes:
 
NXP fuses NXP SRK hashes during manufacturing, and during boot it is verified that only signed binaries
by NXP can be loaded as an ELE fwr to the ELE CPU and these fuse words then set to non-readable?
 
Later, OEM SRK hashes can be added in order to verify bootloader\OS images for OEM usage.
0 Kudos
Reply
3 Replies

2,368 Views
SanderV
Contributor I

Hello,

I have the same question regarding the bootconfig fuses.  According to table 29 in the i.MX93 reference manual, with Boot_mode[3:0] 0010, the boot device is "USDHC1 8-bit eMMC 5.1". However, according to Table 52, with BOOT_CFG[18:17] 00 (eFUSE default); 4 bit eMMC/MMC Bus width. What is the default bus width and can USDHC1 be used to boot from in 4-bit mode id the fuses are set correctly?

Thanks

0 Kudos
Reply

3,338 Views
im93user
Contributor I

[bump]

Hello, can I get a clarification for my questions above?


Thank you

0 Kudos
Reply

2,181 Views
doyayax
Contributor II

The difference is  Normal Boot Mode  vs Boot from Internal Fuses Mode.

You could not use fuse for Normal Boot Mode.

 

 

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-1870363%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3Ei.mx93%20Fusebox%20description%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1870363%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CDIV%3EDear%20NXP%2C%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EI%20have%20a%20few%20issues%20with%20the%20fusebox%20descriptions%20across%20all%20available%20documents%20for%20imx93%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3EGeneral%20questions%3A%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EIMX93RM_rev4%3A%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%22Fuses%20can%20generally%20only%20be%20set%20from%200%20to%201%20and%20the%20most%20common%20failure%20is%20a%201%20appearing%20as%20a%200.%20The%20simplest%20mechanism%20to%20verify%26nbsp%3B%3C%2FDIV%3E%3CDIV%3Ethese%20failures%20is%20redundancy.%20Redundancy%20is%20when%20two%20bits%20are%20OR'd%20together%20so%20that%20if%20either%20is%20set%2C%20then%20the%20output%20value%20is%20a%201.%3C%2FDIV%3E%3CDIV%3EIn%20case%20of%20fuses%20protected%20by%20redundancy%2C%20only%2016%20of%20the%2032%20bits%20are%20available%20(bits%2015%3A0%20are%20automatically%20copied%20to%2031%3A16)%20and%26nbsp%3B%3C%2FDIV%3E%3CDIV%3Echecked%20on%20read.%20This%20allows%20for%20multiple%20programming%20operations%20on%20a%20word%2C%20so%20bits%20can%20be%20configured%20at%20different%20times.%22%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EI%20haven't%20found%20a%20single%20fuse%20in%20the%20fusemap%20xls%20attached%20to%20the%20RM%20or%20in%20the%20security%20RM%20where%20this%20redundancy%20could%20have%20been%20written%20into%3C%2FDIV%3E%3CDIV%3Ethe%20shadowregisters.%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EIs%20that%20redundancy%20something%20that%20is%20handled%20by%20the%20ELE%20fwr%3F%3C%2FDIV%3E%3CDIV%3EWhich%20fuses%20are%20protected%20by%20redundancy%3F%3C%2FDIV%3E%3CDIV%3EDoes%20every%20fuse%20have%20to%20be%20written%20through%20the%20ELE%20API%20or%20are%20there%20any%20other%20fuses%20present%20that%20can%20be%3C%2FDIV%3E%3CDIV%3Eaccessed%20(read%5Cwrite)%20without%20it%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3EQuestions%20regarding%20exact%20fuse%20settings%3A%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3E!BootCFG0!%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3ESD%20Speed%20Selection%2F%20eMMC%20bus%20width%3A%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EIf%20my%20boot%20mode%20fuses%20is%20%22internal%20fuses%22%20and%20bt_fuse_sel%20is%20true%2C%20my%20boot%20mode%20will%20be%3A%3C%2FDIV%3E%3CDIV%3EUSDHC1%208-bit%20eMMC%205.1%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EWhat%20SD%20Speed%20section%20%220b11%20-%208%20bit%20ddr%20(eMMC%204.4)%22%20or%20%220b01%20-%208bit%22%20eMMC%20Bus%20width%20decides%20then%20exactly%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EuSDHC%20IO%20Voltage%20Selection%20%2F%20eMMC%20Speed%20Selection%20%2F%20eMMC%20Bus%20width%3A%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3ECan%20these%20actually%20set%20separately%3F%20Afaik%20HS400%20eMMC%20requires%20all%20of%20these%20to%20be%20set%3A%3C%2FDIV%3E%3CDIV%3E8%20bit%20DDR%2C%201.8%20V%20I%5CO%20%2C%20not%20sure%20what%20high%20speed%20means%20but%20I'm%20guessing%20it%20sets%20the%20clock%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3E!BootCFG1!%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EuSDHC%20Power%20Cycle%20Interval%3C%2FDIV%3E%3CDIV%3EuSDHC%20Power%20Cycle%20Delay%3C%2FDIV%3E%3CDIV%3EPower%20Cycle%20Enable%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EAre%20these%20attached%20to%20the%20secondary%20boot%20offset%20somehow%3F%3C%2FDIV%3E%3CDIV%3EI%20thought%20that%20the%20only%20way%20to%20set%20up%20let's%20say%20a%20fallback%20bootloader%20to%20an%20eMMC%20on%20the%20uSDHC%20is%20to%3C%2FDIV%3E%3CDIV%3Especify%20a%20fixed%20offset%20for%20it%2C%20what%20the%20power%20cycling%20is%5Ccan%20be%20used%20for%20exactly%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EuSDHC%20DLL%20Enable%3C%2FDIV%3E%3CDIV%3EuSDHC%20DLL%20Select%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3ECouldn't%20find%20much%20information%20in%20eMMC%205.1%20reference%20manuals%20for%20this%2C%20how%20does%20that%20work%20exactly%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EWDOG_Enable%3C%2FDIV%3E%3CDIV%3EWDOG_Timeout_Select%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EIs%20the%20WDOG%20needed%20if%20I'm%20using%20a%20fallback%20bootloader%20on%20an%20eMMC%20so%20that%20during%20NORMAL%20boot%20mode%20it%20can%20iterate%3C%2FDIV%3E%3CDIV%3Ethrough%20primary%20bootloader%20-%26gt%3B%20secondary%20bootloader%20-%26gt%3B%20serial%20fallback%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EWhat%20feeds%20the%20WDOG%20HW%20during%20boot%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3E!OEM%20MAC%20ADDRESS!%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E315%20-%20WORD%3C%2FDIV%3E%3CDIV%3E32%26nbsp%3B%20-%20num%20of%20fusebits%3C%2FDIV%3E%3CDIV%3EMAC1_ADDR_31_0%5B31%3A0%5D%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E316%20-%20WORD%3C%2FDIV%3E%3CDIV%3E16%20-%20num%20of%20fusebits%3C%2FDIV%3E%3CDIV%3EMAC1_ADDR_47_32%5B47%3A32%5D%3C%2FDIV%3E%3CDIV%3E16%20-%20num%20of%20fusebits%3C%2FDIV%3E%3CDIV%3EMAC2_ADDR_15_0%5B15%3A0%5D%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E317%20-%20WORD%3C%2FDIV%3E%3CDIV%3E32%26nbsp%3B%20-%20num%20of%20fusebits%3C%2FDIV%3E%3CDIV%3EMAC2_ADDR_47_16%5B47%3A16%5D%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EAccording%20to%20the%20i.MX9%20fusemap%20description%20the%20OEM%20MAC%20addresses%20shall%20be%20stored%20in%20a%20straight-forward%20manner%2C%26nbsp%3B%3C%2FDIV%3E%3CDIV%3Eand%20the%20mainlined%20nvmem%20linux%20drivers%20are%20swapping%20the%20endianness%20the%20MAC%20Addresses%20like%20that.%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EHowever%2C%20the%20security%20reference%20manual%20describes%20the%20exact%20same%20fuses%20the%20following%20way%3A%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E39%20word%203%26nbsp%3B%20MAC1_ADDR_31_0%5B15%3A0%5D%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3BMAC1_ADDR_31_0%5B31%3A16%5D%3C%2FDIV%3E%3CDIV%3E39%20word%204%26nbsp%3B%20MAC1_ADDR_47_32%5B47%3A32%5D%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3BMAC2_ADDR_47_32%5B47%3A32%5D%3C%2FDIV%3E%3CDIV%3E39%20word%205%26nbsp%3B%20MAC2_ADDR_31_0%5B15%3A0%5D%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3BMAC2_ADDR_31_0%5B31%3A16%5D%3C%2FDIV%3E%3CDIV%3E%3CSPAN%3E%26nbsp%3B%20%26nbsp%3B%3C%2FSPAN%3E%3C%2FDIV%3E%3CDIV%3EWhich%20one%20is%20the%20correct%20description%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3E%3CSTRONG%3E!SRK%20HASHES!%3C%2FSTRONG%3E%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3EBased%20on%20the%20RMs%20are%20my%20assumptions%20correct%20regarding%20NXP%20and%20OEM%20SRK%20hashes%3A%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3ENXP%20fuses%20NXP%20SRK%20hashes%20during%20manufacturing%2C%20and%20during%20boot%20it%20is%20verified%20that%20only%20signed%20binaries%3C%2FDIV%3E%3CDIV%3Eby%20NXP%20can%20be%20loaded%20as%20an%20ELE%20fwr%20to%20the%20ELE%20CPU%20and%20these%20fuse%20words%20then%20set%20to%20non-readable%3F%3C%2FDIV%3E%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%3CDIV%3ELater%2C%20OEM%20SRK%20hashes%20can%20be%20added%20in%20order%20to%20verify%20bootloader%5COS%20images%20for%20OEM%20usage.%3C%2FDIV%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2250915%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20i.mx93%20Fusebox%20description%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2250915%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHello%2C%3C%2FP%3E%3CP%3EI%20have%20the%20same%20question%20regarding%20the%20bootconfig%20fuses.%26nbsp%3B%20According%20to%20table%2029%20in%20the%20i.MX93%20reference%20manual%2C%20with%20Boot_mode%5B3%3A0%5D%200010%2C%20the%20boot%20device%20is%20%22USDHC1%208-bit%20eMMC%205.1%22.%20However%2C%20according%20to%20Table%2052%2C%20with%20BOOT_CFG%5B18%3A17%5D%2000%20(eFUSE%20default)%3B%204%20bit%20eMMC%2FMMC%20Bus%20width.%20What%20is%20the%20default%20bus%20width%20and%20can%26nbsp%3BUSDHC1%20be%20used%20to%20boot%20from%20in%204-bit%20mode%20id%20the%20fuses%20are%20set%20correctly%3F%3C%2FP%3E%3CP%3EThanks%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1884056%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20i.mx93%20Fusebox%20description%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1884056%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%5Bbump%5D%3CBR%20%2F%3E%3CBR%20%2F%3EHello%2C%20can%20I%20get%20a%20clarification%20for%20my%20questions%20above%3F%3CBR%20%2F%3E%3CBR%20%2F%3E%3CBR%20%2F%3EThank%20you%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2269358%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20i.mx93%20Fusebox%20description%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2269358%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EThe%20difference%20is%26nbsp%3B%26nbsp%3BNormal%20Boot%20Mode%26nbsp%3B%20vs%26nbsp%3BBoot%20from%20Internal%20Fuses%20Mode.%3C%2FP%3E%3CP%3EYou%20could%20not%20use%20fuse%20for%26nbsp%3BNormal%20Boot%20Mode.%3C%2FP%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E