i.mx8qxp MEK UUU Android Auto OS failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8qxp MEK UUU Android Auto OS failure

Jump to solution
4,429 Views
ET_Dev
Contributor III

Hello 

I am trying to flash the below image on my i.mx8qxp mek board. The process runs to 24% and stops everytime. Please see below log from the command prompt (using windows). Also the logs from serial debug while the process is running. Any pointers to resolve this will be very useful. Thanks. 

13.0.0_1.1.0_AUTO_DEMO_8Q

 

G:\Downloads\nxp_aaos>uuu_imx_android_flash.bat -f imx8qxp -a -e -u c0
This script is validated with uuu 1.4.182 version, it is recommended to align with this version.
dual bootloader is supported
dtbo is supported
dual slot is supported
dynamic partition is supported
vendor_boot is supported
init_boot is supported
generate lines to flash spl-imx8qxp-c0.bin to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash bootloader-imx8qxp-c0.img to the partition of bootloader_a
generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_a
generate lines to flash vendor_boot.img to the partition of vendor_boot_a
generate lines to flash init_boot.img to the partition of init_boot_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_a
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Success 0 Failure 0
G:\Downloads\nxp_aaos>

1:2 15/22 [========> 24% ] FB[-t 600000]: flash super super.img.link

 

Serial Debug:

01-07-2023 18:26:31.861 [RX] - Detect USB boot. Will enter fastboot mode!<CR>

Detect USB boot. Will enter fastboot mode!<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Detect USB boot. Will enter fastboot mode!<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Detect USB boot. Will enter fastboot mode!<CR>

<CR>

MMC erase: dev # 0, block # 8192, count 16 ... <CR>

<CR>

Caution! Your devices Erase group is 0x400<CR>

The erase range would be change to 0x2000~0x23ff<CR>

<CR>

16 blocks erased: OK<CR>

Detect USB boot. Will enter fastboot mode!<CR>

Detect USB boot. Will enter fastboot mode!<CR>

Starting download of 560128 bytes<CR>

....<CR>

downloading of 560128 bytes finished<CR>

writing to partition 'bootloader0'<CR>

Initializing 'bootloader0'<CR>

switch to partitions #1, OK<CR>

mmc0(part 1) is current device<CR>

Writing 'bootloader0'<CR>

<CR>

MMC write: dev # 0, block # 0, count 1094 ... 1094 blocks written: OK<CR>

Writing 'bootloader0' DONE!<CR>

Starting download of 34304 bytes<CR>

<CR>

downloading of 34304 bytes finished<CR>

writing to partition 'gpt'<CR>

Initializing 'gpt'<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Writing 'gpt'<CR>

<CR>

MMC write: dev # 0, block # 0, count 34 ... 34 blocks written: OK<CR>

Writing 'gpt' DONE!<CR>

flash backup gpt image successfully<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

flash target is MMC:0<CR>

The device is already unlocked<CR>

Starting download of 3893248 bytes<CR>

.............................<CR>

downloading of 3893248 bytes finished<CR>

writing to partition 'bootloader_a'<CR>

Initializing 'bootloader_a'<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Writing 'bootloader_a'<CR>

<CR>

MMC write: dev # 0, block # 16384, count 7604 ... 7604 blocks written: OK<CR>

Writing 'bootloader_a' DONE!<CR>

Starting download of 4194304 bytes<CR>

................................<CR>

downloading of 4194304 bytes finished<CR>

writing to partition 'dtbo_a'<CR>

Initializing 'dtbo_a'<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Writing 'dtbo_a'<CR>

<CR>

MMC write: dev # 0, block # 81920, count 8192 ... 8192 blocks written: OK<CR>

Writing 'dtbo_a' DONE!<CR>

Starting download of 67108864 bytes<CR>

..........................................................................<CR>

..........................................................................<CR>

..........................................................................<CR>

..........................................................................<CR>

..........................................................................<CR>

..........................................................................<CR>

....................................................................<CR>

downloading of 67108864 bytes finished<CR>

writing to partition 'vendor_boot_a'<CR>

Initializing 'vendor_boot_a'<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Writing 'vendor_boot_a'<CR>

<CR>

MMC write: dev # 0, block # 393216, count 131072 ... 131072 blocks written: OK<CR>

Writing 'vendor_boot_a' DONE!<CR>

Starting download of 8388608 bytes<CR>

................................................................<CR>

downloading of 8388608 bytes finished<CR>

writing to partition 'init_boot_a'<CR>

Initializing 'init_boot_a'<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Writing 'init_boot_a'<CR>

<CR>

MMC write: dev # 0, block # 360448, count 16384 ... 16384 blocks written: OK<CR>

Writing 'init_boot_a' DONE!<CR>

Starting download of 67108864 bytes<CR>

..........................................................................<CR>

..........................................................................<CR>

..........................................................................<CR>

..........................................................................<CR>

..........................................................................<CR>

..........................................................................<CR>

....................................................................<CR>

downloading of 67108864 bytes finished<CR>

writing to partition 'boot_a'<CR>

Initializing 'boot_a'<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Writing 'boot_a'<CR>

<CR>

MMC write: dev # 0, block # 98304, count 131072 ... 131072 blocks written: OK<CR>

Writing 'boot_a' DONE!<CR>

Starting download of 8192 bytes<CR>

<CR>

downloading of 8192 bytes finished<CR>

writing to partition 'vbmeta_a'<CR>

Initializing 'vbmeta_a'<CR>

switch to partitions #0, OK<CR>

mmc0(part 0) is current device<CR>

Writing 'vbmeta_a'<CR>

<CR>

MMC write: dev # 0, block # 27250688, count 16 ... 16 blocks written: OK<CR>

Writing 'vbmeta_a' DONE!<CR>

Starting download of 16765008 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16765008 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16765008<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16769024 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16765032 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16765032 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16765032<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 19111936 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16765044 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16765044 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16765044<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 17055744 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16765084 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16765084 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16765084<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 17330176 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764992 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764992 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764992<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

Starting download of 16764980 bytes<CR>

..........................................................................<CR>

.....................................................<CR>

downloading of 16764980 bytes finished<CR>

writing to partition 'super'<CR>

sparse flash target is mmc:0<CR>

writing to partition 'super' for sparse, buffer size 16764980<CR>

Flashing sparse image at offset 798720<CR>

Flashing Sparse Image<CR>

........ wrote 16764928 bytes to 'super'<CR>

 

0 Kudos
Reply
1 Solution
4,244 Views
joanxie
NXP TechSupport
NXP TechSupport

1) confirm if your board is use C0

2) try to use the command again and tell me the result

.\uuu_imx_android_flash.bat -f imx8qxp -e -u c0

View solution in original post

0 Kudos
Reply
7 Replies
4,297 Views
ET_Dev
Contributor III

Hello Joan Xie, any pointers on how to fix this issue? 

0 Kudos
Reply
4,334 Views
joanxie
NXP TechSupport
NXP TechSupport

did you use your own board or nxp mek board? and what image do you use? build by yourself or prebuilt image from NXP?

0 Kudos
Reply
4,328 Views
ET_Dev
Contributor III

We are using the following latest Android Auto OS Prebuilt Image from NXP, we are using the NXP MEK board.

13.0.0_1.1.0_AUTO_DEMO_8Q

0 Kudos
Reply
4,296 Views
ET_Dev
Contributor III

Hello Joan Xie,

Do you have any pointers for us, on how to resolve this? 

0 Kudos
Reply
4,245 Views
joanxie
NXP TechSupport
NXP TechSupport

1) confirm if your board is use C0

2) try to use the command again and tell me the result

.\uuu_imx_android_flash.bat -f imx8qxp -e -u c0

0 Kudos
Reply
4,230 Views
ET_Dev
Contributor III

Joan Xie,

 

Thanks that worked and now we are able to boot the OS. Please help understand the difference between the two.

 

uuu_imx_android_flash.bat -f imx8qxp -a -e -u c0

uuu_imx_android_flash.bat -f imx8qxp -e -u c0
0 Kudos
Reply
4,211 Views
joanxie
NXP TechSupport
NXP TechSupport

-a is only flash to the slot a, for more detailed information, pls refer to the able 8. Storage partition

https://www.nxp.com.cn/docs/en/user-guide/Android_Auto_User's_Guide.pdf

0 Kudos
Reply