i.mx8m plus support lpddr4 and lpddr4x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx8m plus support lpddr4 and lpddr4x

ソリューションへジャンプ
5,917件の閲覧回数
zc_tee
Contributor III

Dear all,

May i know does i.mx8M Plus support both LPDDR4 and LPDDR4x RAM?

Thank you.

Regards,

Tee

0 件の賞賛
返信
1 解決策
5,908件の閲覧回数
Yuri
NXP Employee
NXP Employee

@zc_tee 
Hello,

   I've sent You some comments directly.

Regards,
Yuri.

元の投稿で解決策を見る

11 返答(返信)
5,626件の閲覧回数
040869
Contributor I

Could I also get your comment? Interesting usage LPDDR4X >32Gb on own project.

Thanks!

0 件の賞賛
返信
5,807件の閲覧回数
richard_hu
Senior Contributor I

@Yuri 

Could I also get your comment?

We are considering to use LPDDR4X as well.

0 件の賞賛
返信
5,796件の閲覧回数
Yuri
NXP Employee
NXP Employee

@richard_hu 
  Done!

0 件の賞賛
返信
5,909件の閲覧回数
Yuri
NXP Employee
NXP Employee

@zc_tee 
Hello,

   I've sent You some comments directly.

Regards,
Yuri.

4,353件の閲覧回数
amigen-jason
Contributor IV

Yuri,

I'd like the comments as well.  We would like to use an LPDDR4X with the i.MX 8MPlus purely for power savings (not increased bandwidth), if possible. 

 

We currently run LPDDR4 at 800 MHz as our systems do not have intensive memory bandwidth requirements, but do have extreme low power requirements (on battery).

0 件の賞賛
返信
5,005件の閲覧回数
aviad_h
Senior Contributor I

@Yuri 

Can you please share comments 

0 件の賞賛
返信
5,534件の閲覧回数
torus1000
Contributor V

@Yuri 

Could I also get your comment? Thanks!

0 件の賞賛
返信
5,530件の閲覧回数
Yuri
NXP Employee
NXP Employee

@torus1000 
Hello,

   The 8M Plus does not support LPDDR4x.

Regards,
Yuri.

0 件の賞賛
返信
5,750件の閲覧回数
anhui527
Contributor III

Could I also get your comment? thanks.

0 件の賞賛
返信
5,743件の閲覧回数
Yuri
NXP Employee
NXP Employee

@anhui527 
Hello,

  I've sent You comments in Case Number 00328551.

Regards,
Yuri.

0 件の賞賛
返信
5,904件の閲覧回数
zc_tee
Contributor III

Thank you! got your comment already.

Regards,

Tee

0 件の賞賛
返信