i.mx8m plus support lpddr4 and lpddr4x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8m plus support lpddr4 and lpddr4x

Jump to solution
6,223 Views
zc_tee
Contributor III

Dear all,

May i know does i.mx8M Plus support both LPDDR4 and LPDDR4x RAM?

Thank you.

Regards,

Tee

0 Kudos
Reply
1 Solution
6,214 Views
Yuri
NXP Employee
NXP Employee

@zc_tee 
Hello,

   I've sent You some comments directly.

Regards,
Yuri.

View solution in original post

11 Replies
5,932 Views
040869
Contributor I

Could I also get your comment? Interesting usage LPDDR4X >32Gb on own project.

Thanks!

0 Kudos
Reply
6,113 Views
richard_hu
Senior Contributor I

@Yuri 

Could I also get your comment?

We are considering to use LPDDR4X as well.

0 Kudos
Reply
6,102 Views
Yuri
NXP Employee
NXP Employee

@richard_hu 
  Done!

0 Kudos
Reply
6,215 Views
Yuri
NXP Employee
NXP Employee

@zc_tee 
Hello,

   I've sent You some comments directly.

Regards,
Yuri.

4,659 Views
amigen-jason
Contributor IV

Yuri,

I'd like the comments as well.  We would like to use an LPDDR4X with the i.MX 8MPlus purely for power savings (not increased bandwidth), if possible. 

 

We currently run LPDDR4 at 800 MHz as our systems do not have intensive memory bandwidth requirements, but do have extreme low power requirements (on battery).

0 Kudos
Reply
5,311 Views
aviad_h
Senior Contributor I

@Yuri 

Can you please share comments 

0 Kudos
Reply
5,840 Views
torus1000
Contributor V

@Yuri 

Could I also get your comment? Thanks!

0 Kudos
Reply
5,836 Views
Yuri
NXP Employee
NXP Employee

@torus1000 
Hello,

   The 8M Plus does not support LPDDR4x.

Regards,
Yuri.

0 Kudos
Reply
6,056 Views
anhui527
Contributor III

Could I also get your comment? thanks.

0 Kudos
Reply
6,049 Views
Yuri
NXP Employee
NXP Employee

@anhui527 
Hello,

  I've sent You comments in Case Number 00328551.

Regards,
Yuri.

0 Kudos
Reply
6,210 Views
zc_tee
Contributor III

Thank you! got your comment already.

Regards,

Tee

0 Kudos
Reply