i.mx8m how to configure ecspi2 pins as ecspi function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx8m how to configure ecspi2 pins as ecspi function

1,961 次查看
coindu
Contributor IV

Hi anyone:

    I want to pull out the ECSPI2_SCLK ECSPI2_MOSI ECSPI2_MISO ECSPI2_SCLK pins to the SPI function。 configure device tree as follows

pinctrl_ecspi2: ecspi2grp {
fsl.pins = <
MX8MQ_IOMUXC_ECSPI2_SCLK_GPIO5_IO10 0x16
MX8MQ_IOMUXC_ECSPI2_MOSI_ECSPI2_MOSI 0x16
MX8MQ_IOMUXC_ECSPI2_MISO_ECSPI2_MISO 0x16
MX8MQ_IOMUXC_ECSPI2_SCLK_ECSPI2_SCLK 0x1816
>;
}; 

&ecspi1{
fsl,spi-num-chipselects= < 1 >;
cs-gpios = <&gpio5 10 0 > ;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi2 >;
status = "okay";
#address-cells=<1>;
#size-cells=<0>;
spidev@0x00{
#address-cellss=<1>;
#size-cells=<1>;
compatible = "spidev";
spi-max-frequency = <20000000>;
reg = <0>;
};


};

while the ecspi1 in fsl-imx8mq.dtsi "compatible = "fsl,imx6ul-ecspi", "fsl,imx51-ecspi";"

Then i search the compatible in kernel code , the file is drivers/spi/spi-imx.c

but make menuconfig in kernel , can`t choose the configure.

can anybody to tell me how to deal with it.

1 回复

1,481 次查看
igorpadykov
NXP Employee
NXP Employee

Hi coin

for ecspi2 one can look at boundary devices imx8mq-nitrogen8m.dts example
linux-imx6/imx8mq-nitrogen8m.dts at boundary-imx_4.9.x_8mq_ga-pass1-ath10k · boundarydevices/linux-i... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复