i.mx8M mini MIPI-CSI RGB565 raw data copy to RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx8M mini MIPI-CSI RGB565 raw data copy to RAM

ソリューションへジャンプ
930件の閲覧回数
kensu
Contributor V

Hi 

 

We are looking for an MCU/MPU that supports RGB565 16-bit MIPI-CSI.

Our application will require the MIPI-CSI + DMA to store the RGB565 16-bit raw data to RAM and process the raw data through our software.

We need to bypass the HW ISP.

 

Can i.mx8 mini or others support our requirement?

 

Regards

Ken

 

 

タグ(1)
0 件の賞賛
返信
1 解決策
917件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I suggest that you can consider imx8mp or imx8mm, if you don't need ISP, you can use iMX8MM, refer to the RM, 

13.5.1.2 Features
• MIPI D-PHY specification V1.2 (Board Approved)
• Compliant to MIPI CSI2 Specification V1.3 except for C-PHY feature (Board
Approved)
• Support primary and secondary Image format
• YUV420, YUV420 (Legacy), YUV420 (CSPS), YUV422 of 8-bits and 10-bits
• RGB565, RGB666, RGB888
• RAW6, RAW7, RAW8, RAW10, RAW12, RAW14
• All of User defined Byte-based Data packet

 

元の投稿で解決策を見る

1 返信
918件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I suggest that you can consider imx8mp or imx8mm, if you don't need ISP, you can use iMX8MM, refer to the RM, 

13.5.1.2 Features
• MIPI D-PHY specification V1.2 (Board Approved)
• Compliant to MIPI CSI2 Specification V1.3 except for C-PHY feature (Board
Approved)
• Support primary and secondary Image format
• YUV420, YUV420 (Legacy), YUV420 (CSPS), YUV422 of 8-bits and 10-bits
• RGB565, RGB666, RGB888
• RAW6, RAW7, RAW8, RAW10, RAW12, RAW14
• All of User defined Byte-based Data packet