i.mx8 qm - > More than 32bit address page DMA via PCIe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8 qm - > More than 32bit address page DMA via PCIe

Jump to solution
2,696 Views
hcyang1012
Contributor I

We are developing a system with our i.MX8QM based custom board, which transfers large(several MB~GB) data to co-processor through PCIe-DMA.

When we tested DMA performance using our device driver for co-processor, we found that there is a significant performance overhead on dma_map_sg() function, which maps physical address into dma bus address.

Following is how DMA works:

1. User application allocates a buffer.(malloc, std::vector, etc..)

2. Pass the pointer of the buffer via write or read syscall.

3. Syscall handler in our PCI-based custom coprocessor device driver pins page of the buffer into kernel space.

4. Prepare scatter gather list and fill it with page numbers of the pinned page.

5. Call dma_map_sg(), passing the scatter gather list to map the physical address of pinned pages into dma bus address.

6. Run DMA with the filled scatter gather list.

 

In step 5, we found that the swiotlb newly allocates bounce buffer and copying is occurred, which result in significant performance overhead. According to our analysis, this is due to the limitation which DMA can only access under 32 bit address

So we want to know :

1. Why can DMA access <= 32 bit address only? Is it the linux kernel's or i.MX8's limitation?

2. It is very hard to allocate a several KB~MB size buffer <= 4GB area by device driver. Is there any way to avoid to using swiotlb-bounce buffer? For example:

- Using H/W IOMMU

- Unlocking(?) 32-bit address limitation.

- Others.

Thanks in advance.

Best regards

Heecheol Yang.

0 Kudos
Reply
1 Solution
2,497 Views
Yuri
NXP Employee
NXP Employee

@hcyang1012 
Hello,

    I am afraid, right now it is not possible to use the expanded memory.

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
2,557 Views
Yuri
NXP Employee
NXP Employee

@hcyang1012 
Hello,

   The address area, higher 1_0000_0000, which was mentioned as "Used for Mapped IO
external flash devices, extensions space for PCIe" is not supported and generally should
be removed from the Reference Manual(s).

Regards,
Yuri.

0 Kudos
Reply
2,552 Views
hcyang1012
Contributor I

Dear @Yuri 

Thanks for your kind response. 

Then is there any way to use IOMMU in our driver to map those addresses in available addresses?

 

Best Regards 

Heecheol Yang 

0 Kudos
Reply
2,498 Views
Yuri
NXP Employee
NXP Employee

@hcyang1012 
Hello,

    I am afraid, right now it is not possible to use the expanded memory.

Regards,
Yuri.

0 Kudos
Reply