i.mx8 can bus off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8 can bus off

1,945 Views
aksh9354
Contributor I

hello ,

i am using  i.mx8 qm board for the automotive project while testing the things like can communication can bus is going in off state when it doing the communication with host pc but when host pc start the communication first if it sends the message first that time is it is working fine but if first message sending by i.mx board that time can bus is going in the  bus off state

0 Kudos
Reply
2 Replies

1,932 Views
aksh9354
Contributor I

hello while testing i am getting the following errors

when i.mx8 board sent the first message.

can_bus-off.png

 

while testing from host pc towards i.mx8 board communication is fine and working

 

can error_active.png

0 Kudos
Reply

1,941 Views
igorpadykov
NXP Employee
NXP Employee

Hi aksh9354

 

one can test this case on i.MX8QM MEK board with Demo Image

 i.MX 8QuadMax MEK​

use unit tests:

https://source.codeaurora.org/external/imx/imx-test/tree/test/can/doc?h=imx_5.4.70_2.3.0

 

Best regards
igor

0 Kudos
Reply