i.mx7d network switch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx7d network switch

1,666 Views
lcdguru
Contributor II

Hi All,

is there any experience in using the two imx7 lan ports as a network switch?

Thx & BR from Berlin,

Andy

Labels (1)
0 Kudos
Reply
2 Replies

1,579 Views
art
NXP Employee
NXP Employee

When running Linux on the i.MX7D processor, its two Ethernet controllers appear as a separate eth devices. Then, you can bridge them in software using some common Linux methods, e.g. as described here:

https://wiki.archlinux.org/index.php/Network_bridge


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,579 Views
b36401
NXP Employee
NXP Employee

There is nothing special regarding to i.MX. You can run Linux on i.MX7D and configure it as Ethernet switch.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply