i.mx7d network switch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx7d network switch

1,663 次查看
lcdguru
Contributor II

Hi All,

is there any experience in using the two imx7 lan ports as a network switch?

Thx & BR from Berlin,

Andy

标签 (1)
0 项奖励
回复
2 回复数

1,576 次查看
art
NXP Employee
NXP Employee

When running Linux on the i.MX7D processor, its two Ethernet controllers appear as a separate eth devices. Then, you can bridge them in software using some common Linux methods, e.g. as described here:

https://wiki.archlinux.org/index.php/Network_bridge


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,576 次查看
b36401
NXP Employee
NXP Employee

There is nothing special regarding to i.MX. You can run Linux on i.MX7D and configure it as Ethernet switch.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复