i.mx6x h263 encoding configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6x h263 encoding configuration

1,318 次查看
woogeunshin
Contributor II

Hello,

As far as i know, H263 has three header mode that are mode A, B and C.  The rfc2190 is recommend  using mode A.

But, i can't find H263 header mode in VPU library and VPU document.

Could you let met know where can i find it?

Regards,

0 项奖励
回复
2 回复数

1,197 次查看
Yuri
NXP Employee
NXP Employee

  From app team :

  H263 header mode can be configured with the VPU ; please refer to

section 3.2.2.4 (EncHeaderParam) of the VPU API.

https://community.freescale.com/servlet/JiveServlet/download/317735-256858/VPU_API_RM_L3.0.35_1.1.0....

There is no mention of modes but of profiles of which "h.263 - Profile 3" is mentioned (no A,B, or C) .


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,197 次查看
woogeunshin
Contributor II

Hi Yuri,

Thanks for your response. 

Could you give me more detailed information about your mentioned "h.263 - Profile 3"?

I couldn't find it in attached document.

And also, it's not found in the latest manual which is "Rev L3.10.17_1.0.0-ga, 05/2014".

In attached manual,  the struct EncHeaderParam has five members.

typedef struct {

    PhysicalAddress buf;

    int size;

    int headerType;                

    int userProfileLevelEnable;

    int userProfileLevelIndication;

} EncHeaderParam;

Could you let me know which member relates with "h.263 - profiles"?

Regards,

Shin.

0 项奖励
回复