i.mx6ull question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6ull question

1,846 次查看
strive
Contributor I

Dear  Expert:

About i.mx6ull-evk,I have questions below,please help answer,thanks.

1. this picture is from the MCIMX6ULL-CM Page 10:

pastedImage_1.png

a. what function is this signal "GPIO_DVFS"?

b. Is ther a current size requirement about Q702 and Q707? If yes, is the 230mA enough?

c.Q701 is different Q702 and Q707,is there any special?

2. this picture is from the MCIMX6ULL-CM Page 10 too:

pastedImage_2.png

could you tell me whether this circuitry is software watchdog or not?How work?

C738 is a capacity, how is this signal "nWDOG" control UM805RE?

pls help,thanks.

标签 (1)
0 项奖励
回复
4 回复数

1,579 次查看
strive
Contributor I

Dear Expert:

OK,thanks for your support.

BRs

Tom

0 项奖励
回复

1,579 次查看
strive
Contributor I

Dear Expert:

thanks for your answer.

Furthermore:

1. how to  comprehendpastedImage_1.png?

what change is  the DVFS when system reboot?

2. pastedImage_2.pngin this picture,C738 is a capacity,so could you tell me What is the  Electrical property  of the signal  nWDOG,pulse or level,and is this need the software to controll?

thanks for your support.

BRs

Tom

0 项奖励
回复

1,579 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tom

DVFS may lower voltage so processor will not reboot.

For example , if just before reboot  it is under lowest cpu freq setpoint ,

low voltage can not make system boot up at default frequency (as after power-up).

For nWDOG there is no software to control of pulse or level.

~igor

0 项奖励
回复

1,579 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tom

-GPIO_DVFS implements changing arm core voltage for cpufreq driver
-there is no special size requirement for Q701,702, as for Q707 it discharges
VDD_ARM_SOC_IN voltage so may be recommended to use the same type
as used on EVK
-MCIMX6ULL-CM Page 10 implements board reset function used for software
reboot, it is the same solution as for i.MX6Q Sabre SD board spf-27392 p.21,
that is toggle all power board for reliable reboot.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复