i.mx6ull DVFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6ull DVFS

1,332件の閲覧回数
strive
Contributor I

Dear  Expert:

In the IMX6ULLCEC (Rev. 1.1, 05/2017)document,there is a table below:

pastedImage_2.png

But in the Rev. 0, 09/2016,there is a table below:

pastedImage_3.png

About VDD_SOC_IN,one's condition is 900Mhz,another is 528MHz,but the Max Current is the same,that is correct?

Futhermore,in the IMX6ULLIEC document,I can not find the 900MHz version,is there i.mx6ull 900Mhz industry version?

please help,thanks.

0 件の賞賛
返信
1 返信

1,204件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tom

these numbers are very rough estimation, just for reference according to

AN5345 Table 4. Dhrystone benchmark measurement results: 157mA@528MHz
www.nxp.com/docs/en/application-note/AN5345.pdf

 Cortex-A7 core power consumption is 100uW/MHz 

You are right, there is no industrial 900MHz grade, just 800MHz: MCIMX6Y2CVM08AA

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信