i.mx6q openGL update screen abnormal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6q openGL update screen abnormal

1,611 Views
linya
Contributor II

sometime, i.mx6q openGL update screen abnormal.

The screen don't update after call glSwapBuffers();

I need to call glFlush explicitly to avoid this problem.

The render buffer is active but it is not update to screen.

I save the render buffer through glreadpixels after this issue happend.

I check the saved image, the render buffer is update normal , but it is not update to screen.

My software version is:

yocto-fsl imx-3.14.52-1.1.0_ga

GPU library is imx-gpu-viv-5.0.11.p8.4-hfp.bin

GPU work on fb mode. There are no x11 or wayland.

This issue disappear on any one of below situation

1.downgrade the GPU library version to imx-gpu-viv-5.0.11.p8.3-hfp.bin

2.insert some debug message in my render code.

3.Call glFlush function explicitly frame by frame.

Labels (2)
0 Kudos
Reply
1 Reply

1,402 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Lin Ya,

Are you still seeing this behavior? Would it be possible for you to share a test case in order to reproduce this issue?

Regards,

0 Kudos
Reply