Our new project now customer feedback an issue is that usb device disconnect from computer sometimes but it can recover connect immediately.
MCU module: MCIMX6U5EVM10AC
Action:
1. USB eye diagram test is OK ,
2. if USB device connected to computer then remove the usb cable , but measured the USB_OTG_VBUS still output 4.4V(all of the products) .could you please help how to shut down the USB_OTG_VBUS?
Hi Igor:
Today I mearsured the VDDUSB_CAP this voltage is 3.28V , but the specification of i.mx6dl show that this voltage is 3V , and I measured the Demo board is 2.98V . could you please help me to check how can I to regulate it ?
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Zhongwei
suggest to recheck board schematic using IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...
VDDUSB_CAP voltage can be regulated using PMU_REG_3P0n register described in
sect.51.7.2 Regulator 3P0 Register (PMU_REG_3P0n)
i.MX 6Solo/6DualLite Applications Processor Reference Manual
Best regards
igor
Hi Igor:
thanks your good support , i will try it .
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi zhongwei
for usb disconnection problem one can check 24MHz clock stability
and try to use short quality shielded usb cable.
For "shut down the USB_OTG_VBUS" one can check USB_ID signal of
i.MX6 board, when removing the usb cable signal should be high or floating state.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igorpadykov:
Thanks your quick respond .
1. Check 24MHz clock stability----OK , I will check with the crystal manufactor about it .
2. use short usb cable ------our end user's USB cable is about 3m length , but the usb eye diagram test is oK . so the hardware part is good I think .
3. USB_ID signal----how to check the USB_ID signal i can not find this signal . I measured the NXP demo board , if remove the usb cable from computor , the USB_OTG_VBUS is 0V but our is 4.4V .(the demo board MCU model is the same as our product)
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi zhongwei
suggest to change custom board design according to i.MX6Q Sabre SD schematic.
USB_OTG_VBUS can be found on p.11 i.MX6Q Sabre SD schematic:
Best regards
igor
Hi igorpadykov,
Thanks your good support , up is our project about USB signal part .
1. Our USB not with OTG function ,
2. Signal USB_OTG_DN/USB_OTG_DP connect to USB type B connector directly as a device .
3. First time power up ; 1. if not connect USB cable to computer , the USB_OTG_VBUS =0V .
2. if connect USB cable to computer ,the USB_OTG_VBUS =5V , then if remove the
USB cable from computer ,the USB_OTG_VBUS=4.4V( Generallly , if remove the USB
USB cable from computer , the USB_OTG_VBUS should be 0V) so please help to check
why the USB_OTG_VBUS still output 4.4V if remove the USB cable from computer ?
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi zhongwei
had custom board design followed i.MX6Q Sabre SD schematic.
If not, suggest to proceed with help of Commercial Support and Engineering Services | NXP
Best regards
igor