i.mx6UL example code for SDK_2.0_EVK-MCIMX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6UL example code for SDK_2.0_EVK-MCIMX6UL

1,434 Views
hansonhe
NXP Employee
NXP Employee

Dear, do you have below code for i.mx6UL example code for SDK_2.0_EVK-MCIMX6UL? Thanks.

a. AEC CBC hardware encryption and decryption code

b. RNG generation code

c. black  key or red key use example

Labels (1)
0 Kudos
Reply
2 Replies

1,249 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Sorry, but the information you are requesting is treated as confidential ; we cannot discuss this with
you in public anyway, this requires to be handled as a Service Request (SR).

https://community.nxp.com/docs/DOC-329745 

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply

1,249 Views
hansonhe
NXP Employee
NXP Employee

Dear, Yuri,

I do not know the reason why my mail could not log into SR system, could you help submit the request for it? Thanks

0 Kudos
Reply