i.mx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6

1,611 次查看
bande220
Contributor I

error .

标签 (1)
0 项奖励
回复
1 回复

1,356 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Manishkumar

software reboot is not supported and recommended by nxp.

In general one can check some components below critical to rebooting the processor,
if they are in necessary state to support a reboot. Components that fit this
category include (but may not be limited to):
    eMMC memory card (if the hardware RST_B pin is not connected.
    SD Card/socket (if the reset pin is not used to remove power to the SD Card)
    QSPI
    NOR
    LPDDR2/3 memory

For memory may be recommended to run latest version ddr test

i.MX6/7 DDR Stress Test Tool V3.00 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复