i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6

1,585 Views
bande220
Contributor I

error .

Labels (1)
0 Kudos
Reply
1 Reply

1,330 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manishkumar

software reboot is not supported and recommended by nxp.

In general one can check some components below critical to rebooting the processor,
if they are in necessary state to support a reboot. Components that fit this
category include (but may not be limited to):
    eMMC memory card (if the hardware RST_B pin is not connected.
    SD Card/socket (if the reset pin is not used to remove power to the SD Card)
    QSPI
    NOR
    LPDDR2/3 memory

For memory may be recommended to run latest version ddr test

i.MX6/7 DDR Stress Test Tool V3.00 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply