i.mx6 yocto and qt5 Version question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6 yocto and qt5 Version question

1,153 次查看
kangmw086
Contributor III

I installed the YOCTO GATESGARTH.

GATESGATH created the QT5.15.0 toolchain.

Is there no problem with version compatibility if I install the QT5.14 version on UBUNTU and use it by setting SDK?

 

HOST PC : UBUNTU18.04, QT5.14.x

YOCTO QT5.15.x

Is there any problem with cross compile and execution?

 

Should I match the QT5 version installed on my HOST PC with the QT5 version of YOCTO?

 

regards!

0 项奖励
回复
2 回复数

1,145 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello kangmw086,

There will be issues when running the version 5.14 since all the files compile and build for 5.15. But you can test your program its not differ too much from version.

 

Regards

 

 

0 项奖励
回复

1,125 次查看
kangmw086
Contributor III

hi

 

So do you mean that I have to install the QT5.15.x version on the HOST PC and cross-compile it?

 

thangs.

0 项奖励
回复