i.mx6 sabresd parallel port How do I modify the slave address in I2C?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6 sabresd parallel port How do I modify the slave address in I2C?

958件の閲覧回数
ohseohwan
Contributor I

It is tested by connecting an RGB camera to parallel.
I am trying to run the camera by modifying the ov5642.c driver
How do I change the i2c slave address to 0x64?
Is there a place to set the slave address in the kernel source?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

891件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi OH

one can look at "reg" parameter (ov564x: ov564x@3c) in 0v5640 example in

arch/arm/boot/dts/imx6qdl-sabresd.dtsi :

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信