i.mx6 Power Sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx6 Power Sequence

跳至解决方案
3,657 次查看
tollerhecht
Contributor III

In my current project I want to use two parallel camera ports (CSI), powered with 1.8V on NVCC_CSI and NVCC_EIMx ports. The 1.8V supply and the camera ports come from a camera subsystem. When the i.mx6 processor is switched off, the camera system keeps the 1.8V supply and I/Os alive. This means that NVCC_CSI and NVCC_EIMx are still powered with 1.8V, while other i.mx6 power is turned off (except VDD_SNVS_IN). I didn't find anything in the datasheet, which is against this purpose. Anyway, I'm not shure if this is allowed.

Has anyone experiance with that ?

Are the NVCC supplies completely independend ?

Thanks and best regards

标签 (1)
0 项奖励
回复
1 解答
1,949 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Tollerhecht,

As long as VDD_SNVS_IN is powered before any other power supply, there are no other restrictions besides the ones listed in section 4.2.1 of the datasheet (case in which VDDARM_IN and VDDSOC in are supplied separately).

Best regards.

Jorge.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,950 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Tollerhecht,

As long as VDD_SNVS_IN is powered before any other power supply, there are no other restrictions besides the ones listed in section 4.2.1 of the datasheet (case in which VDDARM_IN and VDDSOC in are supplied separately).

Best regards.

Jorge.

0 项奖励
回复