i.mx6 LVDS Screen is different on Android 4.4 vs Android 8.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6 LVDS Screen is different on Android 4.4 vs Android 8.1

1,238 次查看
Proof
Contributor I

Hi

I'm kinda newbish to this, but was super psyched when I was able to install Android on my tablet.

these are the specs of the screen:

Screen Diagonal [mm] 15.6”
Active Area [mm] 344.232 (H) x 193.536 (V)
Pixels H x V 1366(x3) x 768
Pixel Pitch [um] 252 (per one triad) × 252
Pixel Arrangement R.G.B. Vertical Stripe
Display Mode TN Mode, Normally White
White Luminance ( Center ) [cd/m2] 400 cd/m2 (Typ.)
Contrast Ratio 500 (Typ.)
Optical Response Time [msec] 8ms (Typ., on/off)
Nominal Input Voltage VDD [Volt] +5.0 V
LCD Power Consumption [Watt] 2.15 W (Typ.), 2.5 W (Max.)
(all black pattern)
LED Power Consumption [Watt] 7.8 W (Typ.), 8.5 W (Max.)
(all black pattern)
Weight [g] 1250 (Typ.), 1350(Max.)
Physical Size [mm] 363.8(W) X 215.9(H) X 16.85 (D) Typ.
Electrical Interface One channel LVDS
Support Color 16.7M colors (RGB 6-bit + Hi-FRC )

The Problem I'm facing is that on Android 4.4 the screen resolution fit perfectly, while on Android 8 it looks like this:

IMG_20211029_165504.jpg

 

There is also a white glance to it.

 

when running on 4.4 (booted from the SDcard) it looks normal with vibrant colors, so a hardware issue is not causing this white layer

this is my override

setenv extra_bootargs video=mxcfb0:dev=ldb,bpp=16,if=RGB666 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off

 or

 

setenv video video=mxcfb0:dev=ldb,bpp=16,if=RGB666 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off

 

thanks

0 项奖励
回复
2 回复数

1,219 次查看
Proof
Contributor I

Hi wow, thanks for the fast reply

I think I burnt out the screen, it's now just a white screen

0 项奖励
回复

1,233 次查看
igorpadykov
NXP Employee
NXP Employee

Hi William

 

one can try to adjust lcd timings ("display-timings") as in below example

https://variwiki.com/index.php?title=VAR-SOM-MX6_LVDS

 

Best regards
igor