Hi All
I had a question about i.mx53 DDR3 ZQ setting,
in i.mx53_smd flash_header.S
MXC_DCD_ITEM(22, IOMUXC_BASE_ADDR + 0x724, 0x04000000)
The ddr_sel is "10"
but I can find two different description in i.mx53RM,
the smd schematic use 240 ohm ZQ resitor,
which DDR_SEL value is correct?? "00" or "10"
Table 43-2. DDR Output Driver Average Impedance

IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE field descriptions

Sincerely, Max