i.mx53 UART3 incorrect memory map address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53 UART3 incorrect memory map address

1,764 Views
soonwonkim
Contributor I

Hi,

When I check the i.MX53 reference manual (iMX53RM.pdf rev2.1) for UART3 memory map address, in Chapter2 Memeory Map it is 0x5000C000 for UART3 base and 0x53FC4000 for USB (Port PL301). But in Chapter76 all the base address for UART3 is 0x53FC4000. Can you please confirm which address is correct?

Thanks,

Soonwon

Labels (1)
0 Kudos
Reply
2 Replies

1,657 Views
igorpadykov
NXP Employee
NXP Employee

Hi Soonwon

Chapter2 Memeory Map gives correct addresses.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,657 Views
soonwonkim
Contributor I

Thanks a lot for your response!

0 Kudos
Reply