i.mx53 UART3 incorrect memory map address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx53 UART3 incorrect memory map address

1,747件の閲覧回数
soonwonkim
Contributor I

Hi,

When I check the i.MX53 reference manual (iMX53RM.pdf rev2.1) for UART3 memory map address, in Chapter2 Memeory Map it is 0x5000C000 for UART3 base and 0x53FC4000 for USB (Port PL301). But in Chapter76 all the base address for UART3 is 0x53FC4000. Can you please confirm which address is correct?

Thanks,

Soonwon

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,640件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Soonwon

Chapter2 Memeory Map gives correct addresses.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,640件の閲覧回数
soonwonkim
Contributor I

Thanks a lot for your response!

0 件の賞賛
返信