i.mx53 Display reolution setting issue for VGA:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx53 Display reolution setting issue for VGA:

ソリューションへジャンプ
5,265件の閲覧回数
GopiNagaBharath
Contributor IV

Hello,

I have interfaced a VGA (640x480) resolution display on LVDS0 port on i.MX53. The OS used is Linux.

The Display interface works fine, however, with the default resolution of 800x600 which is default configuration.

Can anyone please let me know the procedure for configuring the display resolution to 640x480?

Thanks in advance !

Regards,

Gopi

ラベル(1)
タグ(1)
1 解決策
4,131件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi ,GopiNagaBharath,

   if you use LVDS port, you should add LCD's with 640x480 video mode to ldb.c(linux/drivers/video/mxc/ldb.c)

struct fb_videomode mxcfb_ldb_modedb[] = {

{

  "1080P60", 60, 1920, 1080, 7692,

  100, 40,

  30, 3,

  10, 2,

  0,

  FB_VMODE_NONINTERLACED,

  FB_MODE_IS_DETAILED,},

// {

/* 1024x600 @  , pixel clk @ 51.2MHz */

/* "WSVGA", 60, 1024, 600, 19531,

90, 30,

20, 5,

200, 10,

0,

FB_VMODE_NONINTERLACED,

FB_MODE_IS_DETAILED,},*/

/* {

  "XGA", 60, 1024, 768, 15385,

  220, 40,

  21, 7,

  60, 10,

  0,

  FB_VMODE_NONINTERLACED,

  FB_MODE_IS_DETAILED,},*/

{

/* 1280x800 @ 60 Hz , pixel clk @ 72.4MHz */

"LDB-WXGA",60,1280,800,13812,60,60,20,15,40,3,

FB_SYNC_CLK_LAT_FALL,

FB_VMODE_NONINTERLACED,

0,},

};

1280x800 @ 60 Hz , pixel clk @ 72.4MHz is added by me . you can modify it to 640x480 accroding to your LCD datasheet.

<Note: don't add 3rd one, In this structure, there are only 2 members>

Weidong

元の投稿で解決策を見る

8 返答(返信)
4,131件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

What´s the kernel command line you´ve been using?

0 件の賞賛
返信
4,131件の閲覧回数
GopiNagaBharath
Contributor IV

We are using the below mentioned command,

- setenv bootargs_base 'setenv bootargs console=ttymxc3,115200 console=ttymxc3 video=mxcdi0fb:RGB666,TOSHIBA-XGA di0_primary ldb=single,di=0,ch0_map=SPWG'

Thanks,

Gopi

0 件の賞賛
返信
4,131件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,GopiNagaBharath,

    Try to set u-boot envronment like following ,then test it :

u-boot > setenv bootargs_base 'setenv bootargs console=ttymxc3,115200 console=ttymxc3 video=mxcdi0fb:RGB666,TOSHIBA-XGA di0_primary ldb=di0 video=mxcdi1fb:GBR24,640x480M@60 vga'

<Note: In i.mx53 there 1 IPU module, there are 2 internal parallel interfaces:di0 & di1, di0 & di1 are video source of external interfaces:LVDS0,LVDS1,DISP0 and VGA. The max resolution of IPU is 1080P, so if you use di0 & di1 at the same time, video resolution should be distributed reasonably. >

     From settings in u-boot, video source of TOSHIBA-XGA is from di0, and VGA's is from di1.

R   Regards,

     Weidong

R

0 件の賞賛
返信
4,131件の閲覧回数
GopiNagaBharath
Contributor IV

Hi Weidong,

Thanks for this.

I have tried the same and noticed that the display doesn't work at all, after giving the above setting.

Regards,

Gopi

0 件の賞賛
返信
4,131件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport
Hello,GopiNagaBharath

      Sorry, I forgot that 640x480 resolution mode is not supported in tve.c. See linux/drivers/video/mxc/tve.c

static struct fb_videomode video_modes_vga[] = {

{

/* VGA 800x600 40M pixel clk output */

  "VGA-SVGA", 60, 800, 600, 25000,

  215, 28,

  24, 2,

  13, 2,

  0,

  FB_VMODE_NONINTERLACED,

  FB_MODE_IS_DETAILED,},

{

/* VGA 1024x768 65M pixel clk output */

  "VGA-XGA", 60, 1024, 768, 15384,

  160, 24,

  29, 3,

  136, 6,

  0,

  FB_VMODE_NONINTERLACED,

  FB_MODE_IS_DETAILED,},

  ......

}

Wedong

0 件の賞賛
返信
4,131件の閲覧回数
GopiNagaBharath
Contributor IV

Hi Weidong,

Are these configurations are for LVDS0 port? We are using LVDS0 interface on our board to connect the display with 640x480 resolution.

Regards,

Gopi

0 件の賞賛
返信
4,132件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi ,GopiNagaBharath,

   if you use LVDS port, you should add LCD's with 640x480 video mode to ldb.c(linux/drivers/video/mxc/ldb.c)

struct fb_videomode mxcfb_ldb_modedb[] = {

{

  "1080P60", 60, 1920, 1080, 7692,

  100, 40,

  30, 3,

  10, 2,

  0,

  FB_VMODE_NONINTERLACED,

  FB_MODE_IS_DETAILED,},

// {

/* 1024x600 @  , pixel clk @ 51.2MHz */

/* "WSVGA", 60, 1024, 600, 19531,

90, 30,

20, 5,

200, 10,

0,

FB_VMODE_NONINTERLACED,

FB_MODE_IS_DETAILED,},*/

/* {

  "XGA", 60, 1024, 768, 15385,

  220, 40,

  21, 7,

  60, 10,

  0,

  FB_VMODE_NONINTERLACED,

  FB_MODE_IS_DETAILED,},*/

{

/* 1280x800 @ 60 Hz , pixel clk @ 72.4MHz */

"LDB-WXGA",60,1280,800,13812,60,60,20,15,40,3,

FB_SYNC_CLK_LAT_FALL,

FB_VMODE_NONINTERLACED,

0,},

};

1280x800 @ 60 Hz , pixel clk @ 72.4MHz is added by me . you can modify it to 640x480 accroding to your LCD datasheet.

<Note: don't add 3rd one, In this structure, there are only 2 members>

Weidong

4,131件の閲覧回数
GopiNagaBharath
Contributor IV

Thanks Weidong,

That helped me to successfully change the display resolution to 640x480 !

Regards,

Gopi