i.mx53 Android 4.2.2 400x272 Resolution LCD SurfaceFlinger Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53 Android 4.2.2 400x272 Resolution LCD SurfaceFlinger Error

3,618 Views
cxbere
Contributor I

Hi Everyone,

We are trying porting a 480x272 LCD to our custom i.mx53 board.

This is our LCD structure in mxc_lcdif.c 

...

"0", 60, 480, 272, 111000, 2, 2, 2, 2, 41, 10,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_NONINTERLACED,
0,
},

.....

We have tried part of this structure and it works on Linux, but when we use it on Android 4.2.2. and Linux 30.35, we see some errors like this: (logcat ouput)

I/SurfaceFlinger(15714): SurfaceFlinger is starting
I/SurfaceFlinger(15714): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
D/libEGL (15714): loaded /system/lib/egl/libEGL_imx51.so
D/libEGL (15714): loaded /system/lib/egl/libGLESv1_CM_imx51.so
D/libEGL (15714): loaded /system/lib/egl/libGLESv2_imx51.so
W/imx5x.gralloc(15714): 32bpp setting of Framebuffer catched!
I/imx5x.gralloc(15714): using (fd=16)
I/imx5x.gralloc(15714): id = DISP3 BG
I/imx5x.gralloc(15714): xres = 480 px
I/imx5x.gralloc(15714): yres = 272 px
I/imx5x.gralloc(15714): xres_virtual = 480 px
I/imx5x.gralloc(15714): yres_virtual = 1088 px
I/imx5x.gralloc(15714): bpp = 32
I/imx5x.gralloc(15714): r = 0:8
I/imx5x.gralloc(15714): g = 8:8
I/imx5x.gralloc(15714): b = 16:8
I/imx5x.gralloc(15714): width = 203 mm (60.059113 dpi)
I/imx5x.gralloc(15714): height = 152 mm (45.452629 dpi)
I/imx5x.gralloc(15714): refresh rate = 33.30 Hz
I/hwcomposer(15714): <hwc_get_framebuffer_info,238> Vsync rate 33.299999 fps, frame time 30030030 ns
I/hwcomposer(15714): <hwc_device_open,276>
I/SurfaceFlinger(15714): Using composer version 1.0
W/SurfaceFlinger(15714): getting VSYNC period from fb HAL: 30030030
W/SurfaceFlinger(15714): no suitable EGLConfig found, trying without EGL_FRAMEBUFFER_TARGET_ANDROID
W/SurfaceFlinger(15714): no suitable EGLConfig found, trying without EGL_RECORDABLE_ANDROID
W/GraphicBufferAllocator(15714): WOW! gralloc alloc failed, waiting for pending frees!
W/GraphicBufferAllocator(15714): alloc(480, 272, 1, 00001a00, ...) failed -12 (Out of memory)
D/GraphicBufferAllocator(15714): Allocated buffers:
D/GraphicBufferAllocator(15714): 0x4167b668: 510.00 KiB | 480 ( 480) x 272 | 1 | 0x00001a00
D/GraphicBufferAllocator(15714): 0x4167b7e8: 510.00 KiB | 480 ( 480) x 272 | 1 | 0x00001a00
D/GraphicBufferAllocator(15714): Total allocated (estimate): 1020.00 KB
E/SurfaceFlinger(15714): GraphicBufferAlloc::createGraphicBuffer(w=480, h=272) failed (Out of memory), handle=0x0
E/BufferQueue(15714): [FramebufferSurface] dequeueBuffer: SurfaceComposer::createGraphicBuffer failed
F/libc (15714): Fatal signal 11 (SIGSEGV) at 0x00000020 (code=1), thread 15715 (SurfaceFlinger)
I/DEBUG ( 2350): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
I/DEBUG ( 2350): Build fingerprint: 'Freescale/imx53_smd/imx53_smd:4.2.2/1.1.0-rc3/eng.root.20170203.d2a45e2:eng/dev-keys'
I/DEBUG ( 2350): Revision: '1388577'
I/DEBUG ( 2350): pid: 15714, tid: 15715, name: SurfaceFlinger >>> /system/bin/surfaceflinger <<<
I/DEBUG ( 2350): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 00000020

Could you please share your advice about this problem?

Thanks & Regards,

Labels (3)
0 Kudos
Reply
4 Replies

3,089 Views
cxbere
Contributor I

Thank you for your reply, but I didn't understand. You mean that there is no way to use 480x272 LCD on Linux 3.0.35 and i.mx53, isn't it?

Best Regards.

0 Kudos
Reply

3,089 Views
igorpadykov
NXP Employee
NXP Employee

you can use it, but not using gpu.

Best regards
igor

0 Kudos
Reply

3,089 Views
cxbere
Contributor I

Are there any way to do this, on Android 4.2.2 and Linux 3.0.15? How can I patch for this aim ? Are there any patches, documents, examples or etc?

Could you please share your advice? 

Best Regards

0 Kudos
Reply

3,089 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

unfortunately for that kernel version i.MX53 gpu drivers are not supported

as discussed on

https://community.nxp.com/message/609745?commentID=609745#comment-609745 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply