i.mx51: Kernel Panic while booting from NFS eith uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx51: Kernel Panic while booting from NFS eith uboot

6,216 次查看
MarcoDiVivo87
Contributor I

Hi everybody...

 

I'm trying to boot my kernel from NFS... i have some problem with env. variables on Uboot. I set the following variables :

 

setenv bootargs_nfs
setenv bootcmd_net
setenv bootargs_base
setenv uboot_addr
setenv uboot
setenv kernel
setenv load_uboot
setenv serverip 192.168.0.2
setenv ipaddr 192.168.0.100
setenv nfsroot /home/marco/ltib/rootfs

and add this for DVI(all in one shot) :

setenv bootargs console=ttymxc0,115200 video=mxcdi0fb:RGB24,1024x768M-16@60 di1_primary root=/dev/nfs ip=$(ipaddr) nfsroot=192.168.0.2:$/home/marco/Scrivania/work/ltib/rootfs,v3,tcp

boot

 

this is my printenv list :

 

BBG U-Boot > printenv
bootdelay=3
baudrate=115200
loadaddr=0x90800000
netdev=eth0
ethprime=FEC0
ethact=FEC0
nfssetenv=bootargs consolserverip):,v3,tc
bootcmd=mmc read 0 $(loadaddr) 2000 2000; bootm
serverip=192.168.0.2
ipaddr=192.168.0.100
nfsroot=/tftpboot/fs_imx51
bootargs=console=ttymxc0,115200 video=mxcdi0fb:RGB24,1024x768M-16@60 di1_primary root=/dev/nfs ip=192.168.0.100 nfsroot=192.168.0.2:/home/marco/ltib/rootfs,v3,tp
stdin=serial
stdout=serial
stderr=serial

Environment size: 444/131068 bytes

 

this is the error while booting(last rows) :

 

IP-Config: Complete:                                                                                                                           
     device=eth0, addr=192.168.0.100, mask=255.255.255.0,          gw=255.255.255.255,host=192.168.0.100, domain=, nis-domain=(none),                                                                                           
     bootserver=255.255.255.255, rootserver=192.168.0.2, rootpath=                                                                             
Looking up port of RPC 100003/3 on 192.168.0.2
PHY: 0:00 - Link is Up - 100/Full
Looking up port of RPC 100005/3 on 192.168.0.2
Root-NFS: Server returned error -13 while mounting /home/marco/ltib/rootfs
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)                       
Please append a correct "root=" boot option; here are the available partitions:
1f00            1024 mtdblock0 (driver?)
1f01            3200 mtdblock1 (driver?)
b300         3872256 mmcblk0 driver: mmcblk
b301         3868160 mmcblk0p1
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

 

I can't know what is the problem... i tried to modify with chmod the /rootfs..but nothing...

 

Can anyone help me ??

Thanks a lot !

标记 (1)
0 项奖励
回复
4 回复数

4,260 次查看
MarcoDiVivo87
Contributor I

ok ok ...!

 

now i' m trying to boot with the lcd ;)...

 

thank u a lot !

0 项奖励
回复

4,260 次查看
udragon
Contributor I

Wth the 'nfs' command you load the uImage over nfs at the loadaddr in memory.

The bootm command boots the loaded image

0 项奖励
回复

4,260 次查看
MarcoDiVivo87
Contributor I

Thank u...it works...

Can u tell me the means of the :

setenv bootcmd_nfs 'run bootargs_base bootargs_nfs ; nfs ${loadaddr} ${serverip}:${nfsroot}/boot/uImage;bootm'

 

i've tried to search it on the linux user guide...but nothing....

 

Thank u again!

 

Marco

0 项奖励
回复

4,260 次查看
udragon
Contributor I

Your rootfs points to an nfs which the kernel seems to be unable to mount. 

 

Try this something like this:

 

setenv nfsroot '/tools/rootfs/mx35/rootfs'
setenv bootargs_base 'setenv bootargs console=ttymxc0,115200 ip=${ipaddr}'
setenv bootargs_nfs 'setenv bootargs ${bootargs} root=/dev/nfs nfsroot=${serverip}:${nfsroot},v3,tcp'
setenv bootcmd_nfs 'run bootargs_base bootargs_nfs ; nfs ${loadaddr} ${serverip}:${nfsroot}/boot/uImage;bootm'
setenv bootcmd 'run bootcmd_nfs'
saveenv

 

Also check the obvious, ethernet connection and verify if the nfs server is running on you host

0 项奖励
回复