LTIB MX35 misses amd-gpu module in 2.6.31 kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB MX35 misses amd-gpu module in 2.6.31 kernel

1,501件の閲覧回数
udragon
Contributor I

Hi,

 

I'm building a rootfs based upon ltib vL2.6.31_09.12.01 for the MX35 3stack EVK.

 

When I deploy the rootfs there's no gpu.o/gpu.ko available.

Also in the kernel config there's no option to enable -kernel- GPU support

(The userspace packages amd-gpu-bin-mx35 and libz160-bin are both enabled so there's no issue there)

 

In version 10.2010 of ltib, using L2.6.35, there is a MXC_AMD_GPU option available, however the IPU build for MX35 in this LTIB version is broken so I can't use that LTIB version either.

 

Did any of you manage to enable the amd-gpu kernel driver for MX35 with ltib ?

 

 

Thanks,

 

Christophe

タグ(1)
0 件の賞賛
返信
1 返信

1,381件の閲覧回数
udragon
Contributor I

Got a reply from Freescale that version 102010 and 112011 don't support the i.MX35.

 

I didn't get an answer on the GPU support yet.

0 件の賞賛
返信