i.mx28 system timer/clock problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx28 system timer/clock problem

Jump to solution
5,764 Views
bernhardr_
Contributor I

Hello,

 

While testing the real-time ability of my imx287 I came across some problems.

 

First I created a latency histogram with cyclictest. The histogram I got looked like a comb.

Between 100 and 640us there were vertical lines with a distance of 32us to each other.

 

Then I tried to use ftrace, to get some more latency values.

I got this result:

function_graph: duration 0.000 or 10000.00us

irqsoff:              time 0us or 200000us

sched_event:    timestamp xxx0000

 

The last interesting thing I found out was the result of a simple c-program.

I took two timestamps and calculated the difference:

 

    struct timeval start, stop, diff;     gettimeofday(&start,NULL);     gettimeofday(&stop, NULL);     timersub(&stop, &start, &diff);          clock_gettime(CLOCK_MONOTONIC, &start);     clock_gettime(CLOCK_MONOTONIC, &stop);     diff = time_diff(start, stop);

 

   

I run this program on different machines with this result:

TX28(i.mx287):   mostly 0ns, sometimes 32250ns

RaspberryPi:     1000-5000ns

I7-870:              200-500ns   

 

It looks like a 32us resolution to me.

 

The TX28-Starterkit is simular to the imx28evk.

I use the mainline kernel 3.3 with the tx28 patch.

It seems the patch doesn't change clock/timer code.

Is this phenomenon right for the i.mx28 or is there a bug in the kernel (port)?

Has anybody else recognised this problem using i.mx28?

Maybe someone could try this on the imx28evk.

Where could be the problem?

Original Attachment has been moved to: trace_timer_output.txt.zip

Labels (2)
0 Kudos
Reply
1 Solution
5,044 Views
JackyAtFreescal
Senior Contributor II

That is normal because gettimeofday in imx28 has 31.25usec resolution.

The timer is sourced from 32000Hz clock, see mx28_timer_init() in kernel code.


Regards,

Jacky

View solution in original post

0 Kudos
Reply
4 Replies
5,045 Views
JackyAtFreescal
Senior Contributor II

That is normal because gettimeofday in imx28 has 31.25usec resolution.

The timer is sourced from 32000Hz clock, see mx28_timer_init() in kernel code.


Regards,

Jacky

0 Kudos
Reply
5,044 Views
bernhardr_
Contributor I

Hi,

thanks for your answers,

that's exactly what I am locking for.

I changed the clock source and got a better resolution!

And yes, good point, I should protect my code.

0 Kudos
Reply
5,044 Views
pradipk
Contributor I

Hi Bernhard R.

We are facing same issue!

Could you plz provide details on how you have changed clock source?

sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns

Thank you in advance,

Pradip.

0 Kudos
Reply
5,044 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Bernhard

     Is it possible that the big difference you got on i.MX287 is caused by kernel scheduler? I meant when finishing the collection of start time, then this process is scheduled out, then when it scheduled back, the end time will be much larger. If so, can you try to add some protection to make sure there is no task switch between them, you can try to disable interrupt before executing this code piece.