i.mx28 SPI with ref_io.1 problem!!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx28 SPI with ref_io.1 problem!!!

2,335 Views
grekot
Contributor I

Welcome.
I have a problem with support for SPI in imx287. If the clock source settings "ref_xtal", everything works perfectly. But when the clock signal as a source of law "ref_io.1", while reading the last bit is erroneous, in random bytes.
Has anyone met with this problem and how you solve it?

0 Kudos
Reply
1 Reply

1,485 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi,

 

May I ask how are you configuring the IO1FRAC[5:0] and DIV[8:0] bits in both cases? Do you see a change in the clock frequency when you switch from ref_xtal to ref_io1?

 

Best regards.

Jorge.

0 Kudos
Reply