i.mx25 Serial Download Protocol Statuscodes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx25 Serial Download Protocol Statuscodes

Jump to solution
2,449 Views
fabiansetz
Contributor I

Hi @all,

i get the statuscode 0x56 78 78 56  - 12 3F 3F 12 after sending the write_Memory command (0x02,0x02,...)

what does this returnvalue mean? I cant find it in RM /HAB-Codes?!

Thank you!

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,329 Views
Yuri
NXP Employee
NXP Employee

It should be : 0x56 0x78 0x78 0x56 - 0x12 0x8A 0x8A 0x12.
I do not see any mentions about using 0x3F in HAB boot ROM protocol, sorry.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,330 Views
Yuri
NXP Employee
NXP Employee

It should be : 0x56 0x78 0x78 0x56 - 0x12 0x8A 0x8A 0x12.
I do not see any mentions about using 0x3F in HAB boot ROM protocol, sorry.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,329 Views
fabiansetz
Contributor I

There was an encoding problem with my uart: I only received "Characters" instead of "Bytes" so the MSB was ignored and cut off the rest.

0 Kudos
Reply
2,329 Views
Yuri
NXP Employee
NXP Employee

:-)

0 Kudos
Reply