i.mx25 Serial Download Protocol Statuscodes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx25 Serial Download Protocol Statuscodes

ソリューションへジャンプ
2,495件の閲覧回数
fabiansetz
Contributor I

Hi @all,

i get the statuscode 0x56 78 78 56  - 12 3F 3F 12 after sending the write_Memory command (0x02,0x02,...)

what does this returnvalue mean? I cant find it in RM /HAB-Codes?!

Thank you!

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,375件の閲覧回数
Yuri
NXP Employee
NXP Employee

It should be : 0x56 0x78 0x78 0x56 - 0x12 0x8A 0x8A 0x12.
I do not see any mentions about using 0x3F in HAB boot ROM protocol, sorry.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,376件の閲覧回数
Yuri
NXP Employee
NXP Employee

It should be : 0x56 0x78 0x78 0x56 - 0x12 0x8A 0x8A 0x12.
I do not see any mentions about using 0x3F in HAB boot ROM protocol, sorry.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,375件の閲覧回数
fabiansetz
Contributor I

There was an encoding problem with my uart: I only received "Characters" instead of "Bytes" so the MSB was ignored and cut off the rest.

0 件の賞賛
返信
2,375件の閲覧回数
Yuri
NXP Employee
NXP Employee

:-)

0 件の賞賛
返信