i.Mx6SL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.Mx6SL

1,364件の閲覧回数
phamhuynh
Contributor II

Hello, i have file uimage and zimage then i build kernel, i want to creat file boot.img from both file uimage and zimage, i use command :

~/myandroid/kernel_imx/arch/arm/boot$  ./mkbootimg --kernel zImage --ramdisk ramdisk.img --base 0x80800000 --cmdline 'console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 video=mxc_elcdif_fb:bpp=32 androidboot.hardware=freescale csi' -o new-boot.img

but it appear error:

./mkbootimg: /lib/libc.so.6: version `GLIBC_2.14' not found (required by ./mkbootimg)

Help me for error!, thank everybody!

ラベル(3)
0 件の賞賛
返信
1 返信

1,263件の閲覧回数
Yuri
NXP Employee
NXP Employee

"You also need to use the 10.10 or 11.04 64 bit version of

Ubuntu which are the most tested OS for the Android kk4.4.2

build."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信