i.Mx6 support for SDIO interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx6 support for SDIO interface

2,131 Views
nanjundam
Contributor II

Hi,

I have a question. i.Mx6Q (MCIMX6Q6AVT10AD) has 4 uSDHC controller.

Does all the 4 controller support SDIO interfaces ?

I'm connecting a WLAN interface over SDIO to SD1 controller of i.Mx6Q.

So can anyone tell me does it support SDIO on SD1? Where can I get a proof for the same.

Thanks & Regards,

Nanjunda M 

Labels (1)
0 Kudos
Reply
2 Replies

1,694 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nanjunda M,

Yes, all four uSDHC controllers support MMC/SD/SDIO.

As for connecting a WLAN interface over SDIO to SD1 it is possible and there are third party controllers you may connect to the i.MX6, like for example Silex’s. You may find more information on Silex’s website regarding their modules but there are other WIFI SD modules from third parties that may be able to fulfil your needs.

http://hub.silexamerica.com/unwired/unwired/wi-fi-connectivity-for-i-mx6-platform

I hope this information  helps!

Regards,

0 Kudos
Reply

1,694 Views
nanjundam
Contributor II

Hi,

Thanks for the info, It helps.

Regards,

Nanjunda M

0 Kudos
Reply