i.Mx6 Support for UART interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx6 Support for UART interface

5,260 Views
nanjundam
Contributor II

Hi,

I'm using the i.Mx6 in my design.

I have a requirement to get a RS485 from the UART present in the i.Mx6.

As per data sheet its is possible to use the RS232 Interface to be converted as RS485.

So this conversion of signals need to be done externally or it will be done internal to processor ?

If I have to configure and get an RS485 from one of the UART interface (internal to i.Mx) any external IC to be with it ?

Please help me.

Thanks & Regards,

Nanjunda M

Labels (4)
6 Replies

4,831 Views
mohammedazlum
Contributor IV

Hi,

SN65HVD3086EDR is good for UART TTL level to RS-485 conversion.

Regards,

Azlum

0 Kudos
Reply

4,831 Views
igorpadykov
NXP Employee
NXP Employee

HI Nanjunda

conversion of signals should be done externally

using for example maxim 3430 or similar parts.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,831 Views
nanjundam
Contributor II

Hi igor,

Did you mean that, simple RS485 Transceiver will be required for the UART lines taken out from i.Mx6 to act as RS485 ?

Or is it a converter required from RS232 to RS485  ?

Can you please help me with this confusion.

Thanks & Regards,

Nanjunda M

0 Kudos
Reply

4,831 Views
igorpadykov
NXP Employee
NXP Employee

>Did you mean that, simple RS485 Transceiver will be required for the UART lines taken out from i.Mx6 to act as RS485 ?

yes

Best regards

igor

4,831 Views
nanjundam
Contributor II

Hi Igor,

i have a doubt,

RS485 transceiver has control signals Receive Enable and Driver enable are to be connected to RTS and CTS pins of i.Mx6

So, Do I need to consider them as GPIO pins or I will have retain them as CTS and RTS ?

If retained as CTS and RTS, Which should be connected to REb and DE ?

Please let me know if you know about this.

Thanks & Regards,

Nanjunda M

0 Kudos
Reply

4,831 Views
nanjundam
Contributor II

Can anyone help me with this ASAP?

Regards,

Nanjunda M

0 Kudos
Reply