i.Mx515 Serial port initialisation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx515 Serial port initialisation

1,388 Views
green2
Contributor I

Using WinCE 6.0,

I am trying to get the serial port to communicate with a skyline monitor, I have a touchkit dll which I have added. I am working in windows ce 6.0. I can get debug but I can’t get anything on the other serial port. I am not sure if it is on uart2 or uart2.

 

In the platform reg I have the index set up as 01 and 02, friendly name TX51 COM2 UNIMODEM. I have tried a simple app to see which serial ports I can connect to and I only get the USB ones.

 

Can you shed any light on what might be happening?

0 Kudos
Reply
2 Replies

1,372 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The serial port of Wince and MX51 is UART2 take in mind that the environment variable is BSP_SERIAL_UART2 =1 

You can see more in the driver Third Party -> BSP -> Freescale <Target Platform>: ARMV4I -> Device Drivers > Serial -> UART2 serial port support

Regards

 

 

0 Kudos
Reply

1,368 Views
green2
Contributor I

I don't appear to have the third party/ BSP/ freescale ... directory in my version of wince 6.0.

Where can I get it from? 

0 Kudos
Reply