i.MXRT102X BEE parameter update flow clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT102X BEE parameter update flow clarification

1,018件の閲覧回数
spthx
Contributor II

Hi,

I would like to use the BEE parameter update flow to update the software while using Encrypted XIP Boot on the i.MXRT102X.

For example, if the KIB of the image is
Key: 9e 6c e2 12 35 05 f0 f9 41 2b 9f 08 d2 d0 bc c5
IV : 59 f8 05 45 93 5c c6 8c 57 cc be e4 fa 5d c8 78

and if the start and end of the PRDB's encrypt_region_info are unchanged and the counter is
00 00 00 00 ff 68 db 33 96 5c c2 64 f3 03 73 d5,
how should the BEE register be set?

Should Key be set to BEE_AES_KEY_W0~W3?
And what should be set in BEE_AES_NONCE_W0~W3?

Best Regards,

0 件の賞賛
返信
2 返答(返信)

967件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

As some of the info  of your question is located on the Security reference manual I suggest open a support ticket so I can anwer your questions though e-mail. Support | NXP Semiconductors

Best regards,
Omar

0 件の賞賛
返信

928件の閲覧回数
spthx
Contributor II

@Omar_Anguiano 

Thank you for your reply.
I have created a ticket (case: 00696776).
Please check it.

Best regards,

0 件の賞賛
返信